LS1043A-CONNECT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A-CONNECT

1,175件の閲覧回数
肆加贰
Contributor I

ARM板连接情况.JPG

We use the core board of the LS1043A chip. After power-on, the power supply part is normal. After connecting the CodeWarrior TAP and clicking the A button in the figure, the error in the B area will appear. Our hardware has an error in design, CFG_RCW_SRC0-8 floating, will this hardware error cause this error? Is it possible to modify the Target Initialization file so that the debugger can connect successfully and then debug normally?

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)