LS1043 10GE network port debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043 10GE network port debugging

4,720件の閲覧回数
serenamaya
Contributor I

Hi NXP support team,

In our design, ls1043 and FPGA are connected through xfi, and SFP+ is connected to the FPGA side. If 10 Gigabit network communication needs to be implemented, what changes need to be made to ls1043? The RCW-serdes configuration is 1355. Do I need to configure serdes related registers?

The attachments are u-boot/eth.c and fsl-ls1043a.dts that I modified.

Thanks and best regards,

 

0 件の賞賛
返信
2 返答(返信)

3,871件の閲覧回数
ITMall
Contributor I

have you ever try to find the tech details of this 10gb switch ,it is LS1043 base. Here is the details   https://itmall.sale/product/n9k-c93180yc-fx3/. Hope it helps 

タグ(2)
0 件の賞賛
返信

4,638件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to LS1046ARDB FM1@TGEC2 definition in u-boot source code.

0 件の賞賛
返信