LS1043 10GE network port debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 10GE network port debugging

4,690 Views
serenamaya
Contributor I

Hi NXP support team,

In our design, ls1043 and FPGA are connected through xfi, and SFP+ is connected to the FPGA side. If 10 Gigabit network communication needs to be implemented, what changes need to be made to ls1043? The RCW-serdes configuration is 1355. Do I need to configure serdes related registers?

The attachments are u-boot/eth.c and fsl-ls1043a.dts that I modified.

Thanks and best regards,

 

0 Kudos
Reply
2 Replies

3,841 Views
ITMall
Contributor I

have you ever try to find the tech details of this 10gb switch ,it is LS1043 base. Here is the details   https://itmall.sale/product/n9k-c93180yc-fx3/. Hope it helps 

0 Kudos
Reply

4,608 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to LS1046ARDB FM1@TGEC2 definition in u-boot source code.

0 Kudos
Reply