LS1028A RDB DDR4 Termination Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A RDB DDR4 Termination Voltage

ソリューションへジャンプ
2,204件の閲覧回数
btmeyer
Contributor I

We are using the LS1028A RDB development board. On page 17 of the schematic "spg-39071_a1.pdf" it shows DDR4 terminations tied to VTT_0V6.  I verified on the board itself that this voltage is 0.6V.  However, the Micron DDR4 memory literature states "The I/O buffer has been converted from push-pull to pseudo open drain (POD), as seen in the figure below. By being terminated to VDDQ instead of 1/2 of VDDQ, the size of and center of the signal swing can be custom-tailored to each design’s need."  The data sheet for the DDR4 memory also shows VTT = VDDQ ("test load of 50ohm to VTT = VDDQ") in all situation except the connectivity test mode.  Is VTT=VDDQ correct or is VTT=VDDQ/2 correct?

0 件の賞賛
返信
1 解決策
2,142件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

VTT should be set to VDD/2 and is limited to 0.76V MAX when the power ramp is complete.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,143件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

VTT should be set to VDD/2 and is limited to 0.76V MAX when the power ramp is complete.

0 件の賞賛
返信
2,129件の閲覧回数
btmeyer
Contributor I

Thank you!

0 件の賞賛
返信
2,197件の閲覧回数
btmeyer
Contributor I

A clarification.  On the schematic, VDDQ = 1.2V.

0 件の賞賛
返信