LS1028 + USB3.0 hub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 + USB3.0 hub

1,876件の閲覧回数
sereza1981
Contributor II

Hi!

I'm planning to use LS1028/18 + USB 3.0 hub combination on my PCB. So I have some questions:

1. Have anyone used LS1028/18 + USB 3.0 hub combination?

2. Is there list of checked USB3.0 hub ICs which work without problems with LS1028/18?

3. Or I can use any USB3.0 hub IC with standard Linux driver?

We need industrial grade USB3.0 hub x2, and actually the choice is very short: Texas Instruments TUSB8020B or Cypress CYUSB3314, may be some more, but no on stocks.

Thank you for any information regarding this topic!

Sergej.

タグ(2)
0 件の賞賛
返信
1 返信

1,869件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) There are no known designs.

2) There is no such list - please consider that LS1028A has USB 3.0-compliant controller, so it can be connected to any other USB 3.0-compliant device.

3) Yes.

0 件の賞賛
返信