LS1012a RDB only appears as bootloader?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012a RDB only appears as bootloader?

16,917 Views
nicholashooper
Contributor II

Hi All,

I've gotten a LS1012a RDB and I'm Trying to learn to use it.

The problem I have is the drive doesn't appear when it is plugged in, and only appeared as a drive called BOOTLOADER once I clicked the reset button.

Could anyone help me get the board connected?

I'm sorry is this question has been asked before, but any help is greatly appreciated.

Many thanks in advance,

Nic

Tags (1)
31 Replies

12,513 Views
penman
Contributor II

I have an identical problem but with the LS1046A Reference Design Board:

Cannot connect via serial port connect to the LS1046A RDB, when I connect the console USB to my Windows 10 workstation, I only see a drive labeled "BOOTLOADER" containing one file called bootload.htm, using Windows10 and did not previously disable Windows service 'Storage Services'.

I looked all over for and mbed binary compatible with the LS1046A-RDB and have not found it, is the binary posted above k22fx512_ls1020a_if_mbed.bin.zip in the entry dated Jul 11, 2017 3:50 AM compatible with the LS1046A?

Can someone post the mbed binary for the LS1046A-RDB?

0 Kudos
Reply

12,513 Views
ufedor
NXP Employee
NXP Employee

Yes, the mentioned binary is compatible with the LS1046ARDB.

12,512 Views
angelikileonida
Contributor II

Hi , 

I have the same issue with the bootloader and corrected with the attached binary. 

can you please describe the problem with the bootloader instead of mded serial port so as to know what was the erroneous behavior and when if reproduced?

BR, Angeliki

0 Kudos
Reply

12,515 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> only appeared as a drive called BOOTLOADER

What are contents of the BOOTLOADER?

Have you tried the GSG, "16 Troubleshooting"?

0 Kudos
Reply

12,515 Views
nicholashooper
Contributor II

Under Trouble shooting, It says the D20 LED must be on, however it is not on my board.

0 Kudos
Reply

12,515 Views
ufedor
NXP Employee
NXP Employee

Please provide a clear photo (top) of the powered board with all cables connected.

0 Kudos
Reply

12,515 Views
nicholashooper
Contributor II

DSC_0050.JPG

0 Kudos
Reply

12,515 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> only appeared as a drive called BOOTLOADER

What are contents of the BOOTLOADER?

0 Kudos
Reply

12,512 Views
nicholashooper
Contributor II

There is only a HTML File called "bootload"
Only Bootload.PNG

0 Kudos
Reply

12,509 Views
ufedor
NXP Employee
NXP Employee

Sorry for the delay.

Please copy attached binay image into the BOOTLOADER.

Unplug and plug again the USB cable into the RDB - there should be MBED device instead of the BOOTLOADER:

MBED.png

Also mbed Serial Port should be present in the Device Manager:

2017-07-11_174445.png

12,509 Views
nicholashooper
Contributor II

I'm having an issue now where the mbed drive is disconnecting itself. 

I've made a serial connection in tera term and during booting it froze, the mbed drive dissappeared then re-appeared a few times and the red PORST led is on solid. 

0 Kudos
Reply

12,509 Views
ufedor
NXP Employee
NXP Employee

Is the board brand new?

Have you ever seen consistent console output before the MBED binary was recovered?

0 Kudos
Reply

12,509 Views
nicholashooper
Contributor II

yes it is new, I don't recall seeing console output from this board.

I have also had this disconnect/reconnect problem happen to a FRDM ls1012a board, It will run for a while but eventually the red led will come on and it will freeze.

The only way I've found to get the console running again is to restart my computer, it is possible there is an issue with the computer?

0 Kudos
Reply

12,509 Views
ufedor
NXP Employee
NXP Employee

Please try another computer. Better - with different OS.

0 Kudos
Reply

12,509 Views
nicholashooper
Contributor II

I've given it a try with a windows 7 machine and it worked no problem, it may just be the issue with this computer running windows 10

12,509 Views
zmlopez
Contributor III

There is a problem with mbed and Windows 8 and 10.

You need to download the binary file and then also disable Windows storage services, as is explained in this link:

DAPLink bootloader update | Mbed 

or the problem will happen again.

0 Kudos
Reply

12,509 Views
nicholashooper
Contributor II

Great! it's back up and running again! thank you for all of your help!

0 Kudos
Reply

12,511 Views
ufedor
NXP Employee
NXP Employee

> the drive doesn't appear when it is plugged in

Sorry, what do you mean?

Please provide extended wording and corresponding log.

0 Kudos
Reply

12,511 Views
nicholashooper
Contributor II

Hi Ufedor,

With the device powered, the USB is connected into the laptop, however the device doesn't show up in device manager and it doesn't appear in the "This PC" section as a drive.

What I would expect it to do is appear as a removable drive called "MBED".

I Hope this provides some insight to the problem.

0 Kudos
Reply

12,511 Views
ufedor
NXP Employee
NXP Employee

Please confirm that you have read the QorIQ LS1012A Reference Design Board Getting Started Guide, section 11.

0 Kudos
Reply