LPUART Rx using EDMA on LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPUART Rx using EDMA on LS1021A

1,232 Views
murali417
Contributor I

Hi,

I am trying to enable data transfer from LPUART FIFO buffers to a RAM buffer using EDMA. My ideal case is to achieve this with out interrupting the processor in the whole process. But with the current setup configuration (specified below) I am not able to trigger the DMA. I really appreciate if anyone could take a look at it and see if I am missing any pieces of the puzzle.

DMA MUX:
 
DMAMUX2_CHCFG2 - 0xA0 - Enable and source as LPUART RX1
EDMA Setup:
DMA_CR - 0x0000040C - Enable round robin group and channel arbitration
DMA_ERQ - First tried with 0x0004_0000 and then 0xFFFF_FFFF
TCD : - for 18 - Base address - 0x02C0_1240
 
Source Address - 0x0295_000C - LPUART RX 1 Data Register address
SOFF - 0x0 - Since we do not want to change source address after copy is done
ATTR - 0x0202 - 4bytes
NBYTES - 4
SLAST - 0
DADDR - RAM buffer address
DOFF - 4
CITER - 1
BITER - 1
DLASTSGA - 0
CSR - 0
 
LPUART Setup: Using LPUART1 RX
LPUART1_BAUD - 0x0F20_4036
LPUART1_CTRL - 0x002C_0000
LPUART1_FIFO -  0x0000_0088
LPUART1_WATER - 0x0001_0003
I am guessing that LPUART is not initiating/generating the DMA request when Rx Water level mark is reached.
Thanks,
Murali
0 Kudos
Reply
1 Reply

1,055 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry for delayed response

I do not see anything incorrect in your register settings except LPUART1_FIFO

For the value "LPUART1_FIFO =  0x0000_0088" - if this is a read-back value, than this means FIFO size is only one dataword. In this case setting watermark to 1 is incorrect, LS1021A Reference Manual says:

Receive Watermark
When the number of datawords in the receive FIFO/buffer is greater than the value in this register field, an
interrupt or a DMA request is generated. For proper operation, the value in RXWATER must be set to be
less than the receive FIFO/buffer size as indicated by FIFO[RXFIFOSIZE] and FIFO[RXFE] and must be
greater than 0.

For further debugging please:

1. reconfigure DMAMUX2_CHCFG2 to always-on slot to check if everything is correct with DMA configuration.

2. verify that LPUART reception works and generates interrupt on watermark 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply