Kernel booting problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel booting problem

3,168件の閲覧回数
rajeshtripathi
Contributor I

We have Linux booting on our P2020 based board and trying to use the same kernel on a Kontrom P2020 based board using onboard uboot. I've tried using our dtb file as well as dtb file from Kontron but no progress.

bootargs is console=ttyS0,115200

U-Boot 2009.11 Release GA 2.03 MON (Jul 03 2013 - 21:32:11)

CPU0:  P2020, Version: 2.1, (0x80e20021)

Core:  E500, Version: 5.1, (0x80211051)

Board: Kontron T5310 Rev2 - System Image 0

Reset: 01 Cold Reset, Source: 01 Power Up

PLD:   29 U

I2C:   ready

DRAM:  DDR:   1 GB (DDR3, 64-bit, CL=6, ECC on)

POST memory (fast) PASSED

POST kcs PASSED

FLASH: 256 MB

L2:    512 KB enabled

NAND:  disable_nand is set in env, skipping

VPD:   serial# 9009187384, ethaddr 00:A0:A5:81:6F:22

Net:   eTSEC1

POST i2c PASSED

POST serial PASSED

POST tsec PASSED

POST pci PASSED

POST i2c1 PASSED

autoboot in 3 seconds...

type configured bootstopkey to abort

watchdog stopped

> tftp uImage

Speed: 100, full duplex

Using eTSEC1 device

TFTP from server 192.168.10.1; our IP address is 192.168.10.120

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         ###############################

done

Bytes transferred = 3305745 (327111 hex)

=> tftp 20000000 kontron.dtb

Speed: 100, full duplex

Using eTSEC1 device

TFTP from server 192.168.10.1; our IP address is 192.168.10.120

Filename 'kontron.dtb'.

Load address: 0x20000000

Loading: #

done

Bytes transferred = 8128 (1fc0 hex)

=> bootm 1000000 - 20000000

WARNING: adjusting available memory to 30000000

## Booting kernel  at 01000000 ...

   Verifying Checksum ... OK

## Flattened Device Tree blob at 20000000

   Booting using the fdt blob at 0x20000000

   Uncompressing Kernel Image ... OK

   Loading Device Tree to 00ffb000, end 00ffffbf ... OK

f

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,795件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rajesh Tripathi,


Please refer to the following ramdisk boot environment.

=>setenv ramboot 'setenv bootargs  root=/dev/ram rw console=ttyS0,115200 ramdisk_size=1000000;tftp 0x4000000 rootfs.ext2.gz.u-boot;tftp 0x1000000 uImage.bin;tftp 0x3000000 p2020rdb.dtb;bootm 0x1000000 0x4000000 0x3000000'

=>run ramboot

If your problem remains, please use "pri" command to display and share your u-boot environment.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,795件の閲覧回数
rajeshtripathi
Contributor I

Hi Yiping,

Still no luck. it just hand after loading device tree.

=> printenv

bootcmd=run bootcmd${bootsource}

bootdelay=3

baudrate=115200

loads_echo=1

autoload=no

rootpath=/opt/nfsroot

loadaddr=1000000

setbootargs=setenv bootargs console=ttyS0,${baudrate}

bootcmdprd=watchdog 0; bootp; tftpboot ${loadaddr} t5310-bringup.multi; run setbootargs; bootm ${loadaddr}

disable_nand=yes

initrd_high=20000000

reset_unknown=1

watchdogboot=30

watchdogos=110

disable_rollback=0

stop_posterr=0

rootfs_loadaddr=8000000

test_and_recover=if test ${disable_rollback} = 0; then run recover_flash; fi

check_images=vpdget SERIAL && imcksum e1580000 $rootfs_loadaddr ROOTFS_SIZE ROOTFS_CKSUM && imcksum e0180000 ${loadaddr} OS_SIZE OS_CKSUM

recover_flash=echo Recovering flash ; imgselect.s swap ; reset

bootcmdrecover=run recover_flash

bootcmdflash=echo Booting from flash... ; run check_images && watchdog ${watchdogos} both && boothv ${loadaddr}; run test_and_recover

bootcmddiag=imcksum e4380000 $loadaddr DIAG_SIZE DIAG_CKSUM && watchdog ${watchdogos} && run setbootargs && bootm ${loadaddr}; run test_and_recover

bootcmdnet=watchdog ${watchdogos}; bootp && tftpboot ${loadaddr} ${bootfile} && run setbootargs && bootm ${loadaddr}

stoponposterr=test ${postresult} = 0 || test ${stop_posterr} = 0

early_cmd=watchdog ${watchdogboot}; run stoponposterr

bootsource=flash

clear_env=protect off all; erase e0100000 +40000

clear_config=protect off all; erase e6b80000 +1400000

uboot_flash_update=protect off all && erase e0000000 +80000 && cp.b ${fileaddr} e0000000 ${filesize}

ethaddr=00:A0:A5:81:6F:22

serial#=9009187384

hvbootargs0=linux0:console=ttyS0,${baudrate} macaddr=${ethaddr}

hvbootargs1=linux1:console=ttyS0,${baudrate} macaddr=${ethaddr}

hvbootargs=baudrate=${baudrate}

filesize=327111

fileaddr=1000000

ipaddr=192.168.10.120

serverip=192.168.10.1

eth1addr=00:A0:A5:81:6F:23

eth2addr=00:A0:A5:81:6F:24

stdin=serial

stdout=serial

stderr=serial

ethact=eTSEC1

postresult=0

ramboot=setenv bootargs root=/dev/ram rw console=ttyS0,115200 ramdisk_size=1000000;tftp 0x4000000 rootfs.ext2.gz.u-boot;tftp 0x1000000 uImage;tftp 0x3000000 kontron.dtb;bootm 0x1000000 0x4000000 0x3000000

Environment size: 2088/16379 bytes

=> run ramboot

Speed: 100, full duplex

Using eTSEC1 device

TFTP from server 192.168.10.1; our IP address is 192.168.10.120

Filename 'rootfs.ext2.gz.u-boot'.

Load address: 0x4000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ############################################

done

Bytes transferred = 9224384 (8cc0c0 hex)

Speed: 100, full duplex

Using eTSEC1 device

TFTP from server 192.168.10.1; our IP address is 192.168.10.120

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         ###############################

done

Bytes transferred = 3305745 (327111 hex)

Speed: 100, full duplex

Using eTSEC1 device

TFTP from server 192.168.10.1; our IP address is 192.168.10.120

Filename 'kontron.dtb'.

Load address: 0x3000000

Loading: #

done

Bytes transferred = 8128 (1fc0 hex)

WARNING: adjusting available memory to 30000000

## Booting kernel  at 01000000 ...

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 04000000 ...

   Image Name:   P2020 Ramdisk

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    9224320 Bytes =  8.8 MB

   Load Address: 04000000

   Entry Point:  04000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 03000000

   Booting using the fdt blob at 0x3000000

   Uncompressing Kernel Image ... OK

   Loading Ramdisk to 1f733000, end 1ffff080 ... OK

   Loading Device Tree to 00ffb000, end 00ffffbf ... OK

0 件の賞賛
返信

2,795件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rajesh Tripathi,

It looks that Kontrom u-boot is not compatible with uImage provided in Freescale Linux SDK.

It's better to rebuild Kernel with your required configuration file in Kontrom provided Linux BSP.

Or rebuild u-boot in Freescale Linux SDK environment with Kontrom provided board configuration file.

Thanks,

Yiping

0 件の賞賛
返信

2,795件の閲覧回数
rajeshtripathi
Contributor I

Hello Yiping,

Thanks again for your reply. What in uboot is not compatible with uImage file? Does is has something to do with the way uBoot handles device tree?

I'm using timesys Linux to generate uImage.

Kontron has not provided Linux BSP or any detailed documentation.  Since our board and Kontron board are based on P2020 I was hoping to boot linux with uBoot already on the board as don't want to brick the board by trying to load our uBoot on it.

0 件の賞賛
返信