Issues with TDM_LOOPBACK_TEST within TDM Driver - SDK1.9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues with TDM_LOOPBACK_TEST within TDM Driver - SDK1.9

1,523 次查看
naumgrutman
Contributor II

In reference to  the TDM_LOOPBACK_TEST.c  within  TDM driver of SDK1.9

TDM_LOOPBACK_TEST is not dependable…

The way TDM_LOOPBACK_TEST.c  is written one is bound to get erroneous results claiming that this test is PASSing when indeed it does not… 

Since, if too many poll cycles where shortened by continue;  j variable might never get higher than BUF_COUNT which is equal 5 in which case tdm_check_data() never gets entered thus data is not compared and test returns PASSing results… If one will redefine POLL_COUNT to be 60 or higher I assure you that you will see this test FAILing every time…

 

#define POLL_COUNT         15

#define BUF_COUNT          5

static int poll_count = POLL_COUNT;

...

int poll = 0;

...

while ( ( poll < poll_count ) && !kthread_should_stop() )

   {

   poll++;

   ret = tdm_ch_poll( h_channel1, 10 );

     

   if ( ret != TDM_E_OK )

      continue;

   ...

   ...

   if ( ++j >= BUF_COUNT )

      error_count += tdm_check_data( tx_data[ ( index + 1 ) % BUF_COUNT ], rx_data[ index ] );

 

  index++;

  index = index % BUF_COUNT;

  }

 

...

if ( ( error_count == 0 ) && ( j != 0 ) )

   pr_info( "%s TDM loopback test PASSED!\n", in_loopback ? "Internal" : "External" );

else

   pr_info( "%s TDM loopback test FAILED!\n", in_loopback ? "Internal" : "External" );

 

 

Thanks

Naum

 

0 项奖励
回复
3 回复数

1,205 次查看
naumgrutman
Contributor II

Here is the proof of what I am claiming all along…

Same test is being run every time after power cycle…

It may arbitrarily PASS or FAIL depending on how many

continue; statements the while loop was forced to use…

 

 

Switching control for channel 1 is 20

Operating Fun for channel 2 is a0

Cadence Timer Reg for CH2 before is 7 ff0 0

Cadence Timer Reg for CH2 after is 1 903 20

Switching control for channel 2 is 20

SLIC 2 configuration success

TDM LOOPBACK TEST:

TDM Driver(ID=1)is attached with Adapterfsl_tdm(ID = 0) drv_count=1

TDM LOOPBACK TEST module installed

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 4 ports detected

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

snd-soc-p1022ds: missing/invalid global utils node

ipip: IPv4 over IPv4 tunneling driver

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

Key type dns_resolver registered

/home/ngrutman/QorIQ-SDK-V1.9-20151210-yocto/build_p1020rdb/tmp/work-shared/p1020rdb/kernel-source/drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

snd-soc-p1022rdk: missing/invalid global utils node

ALSA device list:

  No soundcards found.

TDM Loopback test completed... continued=11 and j=4

Internal TDM loopback test PASSED!

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 0)

ata1.00: ATA-8: WDC WD3200BEKT-60PVMR0, 01.01A01, max UDMA/133

ata1.00: 625142448 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata1.00: configured for UDMA/100

scsi 0:0:0:0: Direct-Access     ATA      WDC WD3200BEKT-6 01.0 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 625142448 512-byte logical blocks: (320 GB/298 GiB)

sd 0:0:0:0: [sda] 4096-byte physical blocks

sd 0:0:0:0: Attached scsi generic sg0 type 0

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

 sda: sda1 sda2 sda3 sda4

 

...

...

...

 

Switching control for channel 2 is 20

SLIC 2 configuration success

TDM LOOPBACK TEST:

TDM Driver(ID=1)is attached with Adapterfsl_tdm(ID = 0) drv_count=1

TDM LOOPBACK TEST module installed

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

snd-soc-p1022ds: missing/invalid global utils node

ipip: IPv4 over IPv4 tunneling driver

TCP: cubic registered

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 4 ports detected

Initializing XFRM netlink socket

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

Key type dns_resolver registered

/home/ngrutman/QorIQ-SDK-V1.9-20151210-yocto/build_p1020rdb/tmp/work-shared/p1020rdb/kernel-source/drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

snd-soc-p1022rdk: missing/invalid global utils node

ALSA device list:

  No soundcards found.

TX and RX buffer do NOT match. Err_count:79

TDM Loopback test completed... continued=10 and j=5

Internal TDM loopback test FAILED!

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 0)

ata1.00: ATA-8: WDC WD3200BEKT-60PVMR0, 01.01A01, max UDMA/133

ata1.00: 625142448 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata1.00: configured for UDMA/100

scsi 0:0:0:0: Direct-Access     ATA      WDC WD3200BEKT-6 01.0 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 625142448 512-byte logical blocks: (320 GB/298 GiB)

sd 0:0:0:0: [sda] 4096-byte physical blocks

sd 0:0:0:0: Attached scsi generic sg0 type 0

sd 0:0:0:0: [sda] Write Protect is off

 

0 项奖励
回复

1,205 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Naum Grutman,

Please refer to TDM Driver Working in Internal Loopback mode During Validation , please use the file tdm_loopback_test.c which I provided recently.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,205 次查看
naumgrutman
Contributor II

Hello Yiping,

Thank you for your attention to this issue...

I am out of the office until January 3rd...

I will try your new proposed test as soon as I get back to the office

on Jan 3rd and let you know of the progress...

Meanwhile, I wish Happy New Year...

Thanks again,

Naum

0 项奖励
回复