Issue with SSL_Connect on QEMU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with SSL_Connect on QEMU

1,825件の閲覧回数
navindaga
Contributor I

I'm using QorIQ Linux SDK v1.6 which has openssl version 1.0.1g. The host OS is CentOS 7.

I run QEMU emulation using qemu-system-ppc64 and I have not been able to establish SSL connection to a server. SSL Connection works from the host system but does not work on QEMU.

Any suggestions?

I use openssl s_client to test connection to the server and on QEMU, it reports :

"error:140790E5:SSL routines:SSL23_WRITE:ssl handshake failure:s23_lib.c:177:"

0 件の賞賛
返信
1 返信

1,689件の閲覧回数
navindaga
Contributor I

Any thoughts anybody?

0 件の賞賛
返信