Intermittent LS1012A boot failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Intermittent LS1012A boot failure

2,673件の閲覧回数
aanand
Contributor I

Hello,

We are seeing an intermittent case of boot failure.

Most boards do work. But when it does not boot. It throws:

NOTICE:  DDR Init Done NOTICE:  BL2: v1.5(release):LSDK-19.09-2-ga5d22266c NOTICE:  BL2: Built : 17:57:22, Jun 22 2020 NOTICE:  BL2: Booting BL31

and stops there.

What could be the problem?
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,597件の閲覧回数
ufedor
NXP Employee
NXP Employee

Doublecheck the design referring the QorIQ LS1012A Data Sheet and Design Checklist document.

Using a digital scope ensure that POR levels of all signals corresponds with the requirements of the notes in the Table 1. Pinout list by bus of the LS1012A Data Sheet.

Check power-on supplies ramp rate,  reset signals timings and input clocks behaviour.

Use a debugger to check why the BL31 execution is interrupted.

Pay special attention to the DDR SDRAM operation.

0 件の賞賛
返信

2,597件の閲覧回数
aanand
Contributor I

Thanks ufedor‌ do you have any pointers on how to buy one debugger suitable for this?

0 件の賞賛
返信