IOCONFIG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IOCONFIG

1,751 Views
leonidkurilan
Contributor I

Hello,

In BSDL file for P3041 processor wrote:

  "WARNING: Correct operations of the 1149.6 EXTEST_TRAIN and EXTEST_PULSE    "&
  "require use of the IOCONFIG command with correct setting of IOCONFIG       "&
  "register bits per customer board design. Refer to the Hardware Spec.       "&

Where can I find information about the IOCONFIG register length and configuration bits?

How properly config IOCONFIG register to work with IEEE1149.6 commands?

Original Attachment has been moved to: P3041_R1A_110202.BSD.zip

0 Kudos
Reply
1 Reply

1,537 Views
r8070z
NXP Employee
NXP Employee

Have a great day,


The BSDL file refer to app. note AN3886 which describes IOCONFIG command and bits. This app.note was originally created for P4080 and currently has "peliminary, confidential" status. It requires for NDA.  We cannot place such documents here on community pages. In order to continue please see how Enter a Service Request to discuss confidential information

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply