IOCONFIG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IOCONFIG

1,755件の閲覧回数
leonidkurilan
Contributor I

Hello,

In BSDL file for P3041 processor wrote:

  "WARNING: Correct operations of the 1149.6 EXTEST_TRAIN and EXTEST_PULSE    "&
  "require use of the IOCONFIG command with correct setting of IOCONFIG       "&
  "register bits per customer board design. Refer to the Hardware Spec.       "&

Where can I find information about the IOCONFIG register length and configuration bits?

How properly config IOCONFIG register to work with IEEE1149.6 commands?

Original Attachment has been moved to: P3041_R1A_110202.BSD.zip

タグ(1)
0 件の賞賛
返信
1 返信

1,541件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,


The BSDL file refer to app. note AN3886 which describes IOCONFIG command and bits. This app.note was originally created for P4080 and currently has "peliminary, confidential" status. It requires for NDA.  We cannot place such documents here on community pages. In order to continue please see how Enter a Service Request to discuss confidential information

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信