How to use scatter/gather mem2mem transfer with fsl-qdma driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use scatter/gather mem2mem transfer with fsl-qdma driver

1,884 Views
basudebdas
Contributor I

Hi, I am developing a driver module on LS1046A processor (and Linux OS) and want to use fsl-qdma driver for dma data transfer from memory to memory. I am looking for some reference/documentation on how to use the fsl-qdma driver for this purpose. Looking at the fsl-qdma source code, I see that the current memcpy call only supports one source buffer and one destination buffer. No scatter/gather list support. I want to transfer from a list of buffers to a memory destination. How shall I use source scatter/gather list with this fsl-qdma driver ?  I dont see DMA_SG option also when requesting a channel. Any pointer or advice will be very much appreciated.

0 Kudos
Reply
2 Replies

1,660 Views
Pavel
NXP Employee
NXP Employee

The SG mode has been removed from kernel dma engine driver.

If you want to use SG mode please use the LSDK branch linux-4.9.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,660 Views
gyosunshim
Contributor III

Hi, Pavel Chubakov.

It is a long time ago, but I am facing the same problem, so I will reply with any questions.

I am using LSDK1803, and I read the above and used 4.9 because of SG mode.

Why is SG mode removed in higher versions? Is there a better mod to replace?

Thank you,
Best regards.

Gyosun.

0 Kudos
Reply