T1022 Antipads.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1022 Antipads.

1,503 Views
rampal
Contributor I

I am using T1022 in my design, I want to know what size of antipad will i use on DDR4 DQS lanes and Clock lanes. and also on PCIe and SGMII lanes. Is 28 mil antipads is right?

0 Kudos
Reply
5 Replies

1,436 Views
rampal
Contributor I

Thanks for Pad stack details.

In suggested Reference file also, I am unable to find any antipads .

The problem with 32 mil antipad is, we are loosing ground reference to signals.

BGA pitch in T1022 is 31.5.

Regards,

RAM PAL SINGH

0 Kudos
Reply

1,436 Views
ufedor
NXP Employee
NXP Employee

All requested information can be obtained from the "T104xD4RDB_revA.brd"

0 Kudos
Reply

1,436 Views
rampal
Contributor I

In reference Board files of T1042, there are no antipads in REV PA. However in T1040 reference board rev0 file, 26 mils antipads are drawn. what to do.

0 Kudos
Reply

1,436 Views
ufedor
NXP Employee
NXP Employee

The Design package is:

https://www.nxp.com/downloads/en/printed-circuit-boards/T1042D4RDB-PA_DF.zip 

The file in the package is "T104xD4RDB_revA.brd"

The padstack for the V20D10 is:

Padstack.jpg

0 Kudos
Reply

1,436 Views
ufedor
NXP Employee
NXP Employee

It is reasonable to refer to the PCB layout of T1042D4RDB-PA provided in Design Files available at:

QorIQ® T1040 Reference Design Board | NXP 

Padstack name:   V20D10

drill: 10

pad: 20

antipad: 32

0 Kudos
Reply