How to enable USB OTG for LS1046A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable USB OTG for LS1046A

1,845件の閲覧回数
andreasgeißler
Contributor II

Hello,

We are currently try to use the #OTG feature for USB on the LS1046A. We have added:

- CONFIG_USB_DWC3_DUAL_ROLE=y

- CONFIG_USB_OTG=y

to the kernel defconfig and changed the dr_mode in the device tree to "otg".

When using the USB in "peripheral" mode the USB is working as a mass storage device as expected. but when using "otg" the USB port is not working as host or device.

What steps are needed to enable the OTG? What did we forget or did wrong?

Thanks!

Regards,

Andreas

タグ(1)
0 件の賞賛
返信
1 返信

1,605件の閲覧回数
Pavel
NXP Employee
NXP Employee

Please wait answer on your technical case about this problem.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信