How PBL branches to Boot code (Example boot code is in DDR SRAM)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How PBL branches to Boot code (Example boot code is in DDR SRAM)

2,193件の閲覧回数
sreenatha_reddy
Contributor I

How PBL branches to Boot code (Example boot code is in DDR SRAM)..?

0 件の賞賛
返信
1 返信

2,184件の閲覧回数
Pavel
NXP Employee
NXP Employee

Layerscape processors uses SCRATCHRW2 register value as boot location pointer. See the Section

12.3.53 of LS1043a Reference Manual.

 

Usually RCW file in NXP LSDK contains the following code for u-boot address:

write 0x570600, 0x00000000

write 0x570604, 0x60100000

0 件の賞賛
返信