Fail to install source iso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fail to install source iso

1,423件の閲覧回数
david_huang
Contributor I

my Board :LS1021A

 When I install the source iso and execute the command "./sources/meta-freescale/scripts/host-prepare.sh", I get the error below; and I'm suere my net is well, what should I do then?

"Get:19 http://security.ubuntu.com/ubuntu/ precise-security/main libx11-doc all 2:1.4.99.1-0ubuntu2.3 [2,433 kB]
Err http://security.ubuntu.com/ubuntu/ precise-security/main libx11-doc all 2:1.4.99.1-0ubuntu2.3
Connection failed [IP: 91.189.91.26 80]
Fetched 13.0 kB in 1min 15s (172 B/s)
Failed to fetch http://us.archive.ubuntu.com/ubuntu/pool/main/s/slang2/libslang2-dev_2.2.4-3ubuntu1_amd64.deb Something wicked happened resolving 'us.archive.ubuntu.com:http' (-5 - No address associated with hostname)
Failed to fetch http://us.archive.ubuntu.com/ubuntu/pool/main/libc/libcaca/libcaca-dev_0.99.beta17-2.1ubuntu2_amd64.... Something wicked happened resolving 'us.archive.ubuntu.com:http' (-5 - No address associated with hostname)
Failed to fetch http://security.ubuntu.com/ubuntu/pool/main/libx/libx11/libx11-dev_1.4.99.1-0ubuntu2.3_amd64.deb Connection failed [IP: 91.189.91.23 80]
Failed to fetch http://security.ubuntu.com/ubuntu/pool/main/libs/libsdl1.2/libsdl1.2-dev_1.2.14-6.4ubuntu3.1_amd64.d... Connection failed [IP: 91.189.88.161 80]
Failed to fetch http://security.ubuntu.com/ubuntu/pool/main/libx/libx11/libx11-doc_1.4.99.1-0ubuntu2.3_all.deb Connection failed [IP: 91.189.91.26 80]
Failed to fetch http://us.archive.ubuntu.com/ubuntu/pool/main/s/screen/screen_4.0.3-14ubuntu8_amd64.deb Connection failed [IP: 91.189.91.26 80]
E: Unable to fetch some archives, maybe run apt-get update or try with --fix-missing?
ERROR: Fail to install pkgs on host! See message above...
"

0 件の賞賛
返信
1 返信

1,188件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

According to error log you submitted, your Linux workstation can not connect to server with Ubuntu security updates. This problem is specific to your network settings and not related to our SDK. Please contact your IT team for support.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信