FMAN Microcode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FMAN Microcode

1,897 Views
kmanjushree
Contributor I

Hi,

If i need to load the FMAN microcode to T1040RDB then i will copy the microcode from NOR flash to FMan controller Configuration Data Download Registers using the fm_upload_ucode function. The first step in the fm_upload_ucode function is

1. /* enable address auto increase */
out_be32(&imem->iadd, IRAM_IADD_AIE);

2.  /* write microcode to IRAM */
for (i = 0; i < size / 4; i++)
out_be32(&imem->idata, (be32_to_cpu(ucode[i])));

As per the DPAA manual, imem->iadd is FMCDADDR i.e address register. So '0' bit corresponds to Auto increment enable and 1-31 bits is the address.

1. Which address does 1-31 bits point to ?

2. Do i need to specify some address in 1-31 bits so that the microcode gets copied to that location?

3. Or does it point to 0th location?

Thanks

Manjushree 

0 Kudos
Reply
1 Reply

1,808 Views
ufedor
NXP Employee
NXP Employee
0 Kudos
Reply