Error with Management Complex

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error with Management Complex

2,176件の閲覧回数
davehill
Contributor II

I am seeing an error with the Management Complex when booting uboot on my ls2088a

fsl-mc: Booting Management Complex ... WARNING: Firmware returned an error (GSR: 0x51)
Error: Timeout waiting for MC response
fsl-mc: ERROR: Firmware version check failed (error: -110)

I *think* this is because the dtb is not in memory.

I have been searching the documentation but I seem to be missing how I am get the file which I assume is

fsl-ls2088a-rdb.dtb

loaded in.

I do see a section of re-flashing the u-boot which I have done using:

=> ext2load scsi 0:2 a0000000 firmware_ls2088ardb_uboot_norboot.img
=> protect off 584000000 +$filesize && erase 584000000 +$filesize && cp.b a0000000 584000000 $filesize
=> qixis_reset altbank

Any suggestions as to what I am missing ?

2 返答(返信)

1,903件の閲覧回数
davehill
Contributor II

It seems there is problem with fsl_mc lazyapply in 17.12

Converting to "apply" using mcinitcmd solved the issue for me.

setenv mcinitcmd 'fsl_mc start mc 0x580a00000 0x580e00000 && fsl_mc apply dpl 0x580d00000'

saveenv

0 件の賞賛
返信

1,903件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) Which exactly board is in question?

If it is the LS2088ARDB - ensure that on-board configuration switches are in default positions.

2) Provide the NOR Flash programming log corresponding to the mentioned re-flashing commands and complete U-Boot booting log as textual attachments.

0 件の賞賛
返信