Encoding method used in LS1012A in SGMII mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Encoding method used in LS1012A in SGMII mode

2,160 次查看
minalnemade
Contributor II

Hi,

As we want to used SGMII mode for Ethernet communication in our custom board. So we want to know which encoding (8b10b/NRZ/4b5b) method supported by LS1012A MAC?

regards

Minal

0 项奖励
回复
1 回复

2,030 次查看
ufedor
NXP Employee
NXP Employee

SGMII is a non-IEEE-standard mode of communication (defined by Document ENG-46158 Serial-GMII Specification from Cisco Systems) between the MAC and PHY that allows for copper 10/100/1000BASE-T (IEEE Std 802.3ab™) operation.
The SGMII specification is closely related to 1000Base-X in that each utilizes the same Physical Coding Sublayer (PCS) and Physical Medium Attachment (PMA) layers as is defined by 1000Base-X 802.3 Clause 36.

0 项奖励
回复