Enabling GPIO2 on T1020.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling GPIO2 on T1020.

2,003件の閲覧回数
henryeng
Contributor I

I have configured the RCW to use GPIO2 instead of SPI and SDHC.  What else do I need to change to to get GPIO working?  Any u-boot setup required?

0 件の賞賛
返信
3 返答(返信)

1,879件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Henry Eng,

I do not know other change, what issue do you have? Could it work?

Regards

Lunmin

0 件の賞賛
返信

1,879件の閲覧回数
henryeng
Contributor I

Thanks for the reply.  It is working as advertised.  I was just using the wrong gpio numbers from the command line when I tested it.  I should have looked at the /sys/class/gpio/gpiochipxxx more carefully.

0 件の賞賛
返信

1,879件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Thanks for your feedback.

0 件の賞賛
返信