ECC algorithm of DDR SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC algorithm of DDR SDRAM

Jump to solution
3,960 Views
yansongzhu
Contributor III

What is the ECC algorithm of DDR SDRAM on P2020 platform? It seems not the normal Hamming code.

Tags (1)
1 Solution
3,548 Views
ufedor
NXP Employee
NXP Employee

The ECC is a (72,64) Hsiao odd-weight-column code which is modified(shortened) (127,120) Hamming code - refer to the following document (Figure 3, (c)):

https://pdfs.semanticscholar.org/dd97/ac9c9d9267793054aa38782f03342e4ccb32.pdf 

View solution in original post

1 Reply
3,549 Views
ufedor
NXP Employee
NXP Employee

The ECC is a (72,64) Hsiao odd-weight-column code which is modified(shortened) (127,120) Hamming code - refer to the following document (Figure 3, (c)):

https://pdfs.semanticscholar.org/dd97/ac9c9d9267793054aa38782f03342e4ccb32.pdf