Does the T2080 chip support the Rionet driver?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the T2080 chip support the Rionet driver?

2,419 次查看
liguofa
Contributor III

Does the T2080 chip support the Rionet driver? We use yocto 2.0. If there is a relevant reference demo? Or related documents? thank you for your help.khumphri‌MandarDeactivated userdhavalRHinnen

0 项奖励
回复
3 回复数

2,112 次查看
liguofa
Contributor III

yipingwang‌dhavalT-Series

1.Do you mean that T2080 only supports usdpaa lib to control srio?
2.In the beginning, we actually wanted to verify the interconnectivity 
  of the SRIO network and 10G network. Start by considering RIONET.
3.We want to use the T2080 chip and Broadcom 10G switch chip to achieve 
the following diagram function, can give some valuable suggestions, 
thanks very much.Looking forward to your reply, can fra and sra achieve this function?
nxp.jpeg
0 项奖励
回复

2,112 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li guofa,

T2080 processor integrates RMAN not RMU.

RIONET driver in Linux Kernel only supports RMU.

SDK 2.0 supports RMAN in USDPAA application(FRA), please refer to USDPAA FRA user manual provided in Submit Form, QorIQ SDK v2.0-1703 Documentation->Linux User Space->USDPAA Application->NXP USDPAA FRA User Manual.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,079 次查看
pengyingzhong
Contributor I

hello @yipingwang .I have a question.

T2080 has two srio ports directly connected to two fpga respectively. At this time, T2080 will receive two fpga doorbells. The official fra example only supports a single port. May I ask if a T2080 uses two ports at the same time.Examples of linux version?

0 项奖励
回复