Difference between Active Debug Context and Project-specified debug contest in Codewarrior Flash Programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between Active Debug Context and Project-specified debug contest in Codewarrior Flash Programmer

ソリューションへジャンプ
4,920件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I am using Codewarrior Flashprogrammer  version 10.7 for flash the images to T4160 Machine. After everything done, before execute I seen two type of Debug Context. Execute work after select the Projetc-specified debug context (Texst1_core00_RAM_T4160_Download).

I don know what is the difference and which one I want to use for flashing?  

Chosse Target Task file -> Change Run Configuration -> Select Run Configuration and Click -> ok in Target Task Pop Window.

pastedImage_1.png

If it possible, Please send to appropriate steps for flash by using Codewarrior Flashprogrammer version 10.7. Thank you for all! 

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
1 解決策
4,730件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply and Please Ignore this Thread.

Regards,

VinothS

Regards,
Vinothkumar Sekar

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,730件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

What are the configuration is must for flash using Codewarrior Flashprogrammer?

Please give some details and Thank you for all your support.

Thanks & Regards,

VinothS 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
4,730件の閲覧回数
ufedor
NXP Employee
NXP Employee

Active Debug Context (= active debug session) is:

<> debug connection was established and is active

and

<> processor initialization script was executed

During a project creation it is possible to check Debug Configurations "Connect", "Download", "Connect SRAM" and "Download SRAM" - each of them can establish debug session required for the Flash Programmer.

Latter two can be used if SDRAM operation is unstable.

0 件の賞賛
返信
4,725件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply.

I got some error while flashing and I tried the online solutions also. But, still I got the error by using Codewarrior Flashprogrammer. 

I set unprotect in action but, I got error protect/unprotect not support and why I am setting this because of Protection Sector Error.  

And also I attached the error log and flash programmer pdf document for your reference. Thanks for your support.


Error: Erase failed. Flash driver reports the following error(s): Sector Protection Error
Error: Erase failed. Flash driver reports the following error(s): Sector Protection Error

Error: Protect/Unprotect not supported on this device.
Error: Protect/Unprotect not supported on this device.

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
4,725件の閲覧回数
ufedor
NXP Employee
NXP Employee

What is the "GL01GS10FHI_new" in the Flash Error.txt?

0 件の賞賛
返信
4,730件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply and Please Ignore this Thread.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信