Default Root Password on LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Default Root Password on LS1043ARDB

15,075件の閲覧回数
donberkowitz
Contributor II

I built a kernel using fsl-image-kernelitb using the 0.5 SDK and unlike the other builds, the root password is not null.  I have tried all the usual default passwords and none of them work.  What is the default password?

0 件の賞賛
返信
8 返答(返信)

9,142件の閲覧回数
ericdujardin
Contributor I

For the poor souls who might come around here with the same pain, I just had some luck with user/user. It is in fact documented in https://github.com/nxp-imx/meta-nxp-desktop.

12,147件の閲覧回数
addiyi
NXP Employee
NXP Employee

Default pass for root user is root.

Adrian

0 件の賞賛
返信

12,147件の閲覧回数
donberkowitz
Contributor II

I have tried "root" and it does not work.

12,148件の閲覧回数
ufedor
NXP Employee
NXP Employee

Freescale Linux LS1043A SDK, Rev. A

LLog.png

0 件の賞賛
返信

12,148件の閲覧回数
donberkowitz
Contributor II

Did you read the prior reply?  I have tried user root, password root.  IT DOES NOT WORK.  Please see the initial question for  a precise description of the build in the unit.

12,148件の閲覧回数
donberkowitz
Contributor II

I still have not received a reply on this.  I am wondering if there could be a problem with the serial line configuration.  I would not think so, since it does display "root" when I type "root".

The dialog is below:

Poky (Yocto Project Reference Distro) 1.6.1 ls1043ardb /dev/ttyS0

ls1043ardb login: root

Password:

Login incorrect

ls1043ardb login:

Configuration is below:

=>

baudrate=115200

bootargs=console=ttyS0,115200 root=/dev/ram0 rw rootdelay=5

bootcmd=ext2load mmc 0 a0000000 $itb && bootm a0000000

bootdelay=10

console=ttyAMA0,115200n8

eth1addr=00:04:9F:03:DD:12

eth2addr=00:04:9F:03:DD:13

eth3addr=00:04:9F:03:DD:14

eth4addr=00:04:9F:03:DD:15

eth5addr=00:04:9F:03:DD:16

eth6addr=00:04:9F:03:DD:17

ethact=FM1@DTSEC3

ethaddr=00:04:9F:03:DD:11

ethprime=FM1@DTSEC3

fdt_high=0xffffffffffffffff

filesize=2185783

fman_ucode=60300000

hwconfig=fsl_ddr:bank_intlv=auto

initrd_high=0xffffffffffffffff

itb=kernel-fsl-ls1043a-rdb.dtb-ls1043ardb-20160222124800.itb

kernel_addr=0x100000

kernel_load=0xa0000000

kernel_size=0x2800000

kernel_start=0xa0000000

loadaddr=0x80100000

ramdisk_addr=0x800000

ramdisk_size=0x2000000

stderr=serial

stdin=serial

stdout=serial

Environment size: 842/8188 bytes

=>

0 件の賞賛
返信

12,148件の閲覧回数
addiyi
NXP Employee
NXP Employee

Try with:

bootargs root=/dev/mmcblk0p1 rw rootdelay=5 console=ttyS0,115200

With your setting it looks that you load filesystem from ram0.

Adrian

0 件の賞賛
返信

12,148件の閲覧回数
donberkowitz
Contributor II

Hi Adrian,

When I change the parameters to boot directly from the SD chip, the kernel crashes – see below.

Thanks,

Don

=> printenv

baudrate=115200

bootargs=console=ttyS0,115200 root=/dev/ram0 rw rootdelay=5

bootcmd=ext2load mmc 0 a0000000 $itb && bootm a0000000

bootdelay=10

console=ttyAMA0,115200n8

eth1addr=00:04:9F:03:DD:12

eth2addr=00:04:9F:03:DD:13

eth3addr=00:04:9F:03:DD:14

eth4addr=00:04:9F:03:DD:15

eth5addr=00:04:9F:03:DD:16

eth6addr=00:04:9F:03:DD:17

ethact=FM1@DTSEC3

ethaddr=00:04:9F:03:DD:11

ethprime=FM1@DTSEC3

fdt_high=0xffffffffffffffff

filesize=2185783

fman_ucode=60300000

hwconfig=fsl_ddr:bank_intlv=auto

initrd_high=0xffffffffffffffff

itb=kernel-fsl-ls1043a-rdb.dtb-ls1043ardb-20160222124800.itb

kernel_addr=0x100000

kernel_load=0xa0000000

kernel_size=0x2800000

kernel_start=0xa0000000

loadaddr=0x80100000

ramdisk_addr=0x800000

ramdisk_size=0x2000000

stderr=serial

stdin=serial

stdout=serial

Environment size: 842/8188 bytes

=> setenv bootargs 'root=/dev/mmcblk0p1 rw rootdelay=5 console=ttyS0,115200'

=> saveenv

Saving Environment to MMC...

Writing to MMC(0)... done

=>

U-Boot SPL 2015.01QorIQ-SDK-V1.7+gc297f5b (Jan 22 2016 - 13:25:02)

Initializing DDR....

U-Boot 2015.01QorIQ-SDK-V1.7+gc297f5b (Jan 22 2016 - 13:25:02)

Clock Configuration:

CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz

CPU3(A53):1600 MHz

Bus: 400 MHz DDR: 1600 MT/s FMAN: 500 MHz

Reset Configuration Word (RCW):

00000000: 08100010 0a000000 00000000 00000000

00000010: 14550002 80004012 60040000 c1002000

00000020: 00000000 00000000 00000000 00038800

00000030: 00000000 00001100 00000096 00000001

Board: LS1043ARDB, boot from SD

CPLD: V1.4

PCBA: V2.0

SERDES Reference Clocks:

SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ

I2C: ready

DRAM: Detected UDIMM Fixed DDR on board

2 GiB (DDR4, 32-bit, CL=11, ECC off)

Using SERDES1 Protocol: 5205 (0x1455)

fman_port_enet_if:71: port(FM1_DTSEC3) is OK

fman_port_enet_if:77: port(FM1_DTSEC4) is OK

Flash: 128 MiB

NAND: 512 MiB

MMC: FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: disabled

PCIe2: Root Complex no link, regs @ 0x3500000

PCIe3: Root Complex no link, regs @ 0x3600000

In: serial

Out: serial

Err: serial

Net: Fman1: Uploading microcode version 106.4.15

FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 , FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1

Hit any key to stop autoboot: 0

35149699 bytes read in 3766 ms (8.9 MiB/s)

    1. Loading kernel from FIT Image at a0000000 ...

Using 'config@1' configuration

Trying 'kernel@1' kernel subimage

Description: ARM64 Linux kernel

Type: Kernel Image

Compression: gzip compressed

Data Start: 0xa00000dc

Data Size: 4408289 Bytes = 4.2 MiB

Architecture: AArch64

OS: Linux

Load Address: 0x80080000

Entry Point: 0x80080000

Verifying Hash Integrity ... OK

    1. Loading ramdisk from FIT Image at a0000000 ...

Using 'config@1' configuration

Trying 'ramdisk@1' ramdisk subimage

Description: LS1043 Ramdisk

Type: RAMDisk Image

Compression: uncompressed

Data Start: 0xa043b540

Data Size: 30711544 Bytes = 29.3 MiB

Architecture: AArch64

OS: Linux

Load Address: unavailable

Entry Point: unavailable

Verifying Hash Integrity ... OK

    1. Loading fdt from FIT Image at a0000000 ...

Using 'config@1' configuration

Trying 'fdt@1' fdt subimage

Description: Flattened Device Tree blob

Type: Flat Device Tree

Compression: uncompressed

Data Start: 0xa0434574

Data Size: 28481 Bytes = 27.8 KiB

Architecture: AArch64

Verifying Hash Integrity ... OK

Loading fdt from 0xa0434574 to 0x90000000

Booting using the fdt blob at 0x90000000

Uncompressing Kernel Image ... OK

reserving fdt memory region: addr=80000000 size=10000

Using Device Tree in place at 0000000090000000, end 0000000090019f40

Starting kernel ...

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Linux version 3.19.3+ (don@don-LTJ843) (gcc version 4.8.3 20140401 (prerelease) (Linaro GCC 4.8-2014.04) ) #2 SMP PREEMPT Mon Feb 1 08:46:56 PST 2016

CPU: AArch64 Processor revision 4

Detected VIPT I-cache on CPU0

efi: Getting EFI parameters from FDT:

efi: UEFI not found.

Reserved memory: initialized node bman-fbpr, compatible id fsl,bman-fbpr

Reserved memory: initialized node qman-fqd, compatible id fsl,qman-fqd

Reserved memory: initialized node qman-pfdr, compatible id fsl,qman-pfdr

cma: Reserved 16 MiB at 0x00000000fb000000

psci: probing for conduit method from DT.

psci: PSCIv0.2 detected in firmware.

psci: Using standard PSCI v0.2 function IDs

PERCPU: Embedded 14 pages/cpu @ffffffc07fd8f000 s18880 r8192 d30272 u57344

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 515592

Kernel command line: root=/dev/mmcblk0p1 rw rootdelay=5 console=ttyS0,115200

log_buf_len individual max cpu contribution: 4096 bytes

log_buf_len total cpu_extra contributions: 12288 bytes

log_buf_len min size: 16384 bytes

log_buf_len: 32768 bytes

early log buf free: 14628(89%)

PID hash table entries: 4096 (order: 3, 32768 bytes)

Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)

Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)

Memory: 1948764K/2095104K available (6497K kernel code, 460K rwdata, 2204K rodata, 284K init, 709K bss, 129956K reserved, 16384K cma-reserved)

Virtual kernel memory layout:

vmalloc : 0xffffff8000000000 - 0xffffffbdbfff0000 ( 246 GB)

vmemmap : 0xffffffbdc0000000 - 0xffffffbfc0000000 ( 8 GB maximum)

0xffffffbdc2000000 - 0xffffffbdc3ff8000 ( 31 MB actual)

PCI I/O : 0xffffffbffa000000 - 0xffffffbffb000000 ( 16 MB)

fixed : 0xffffffbffbdfd000 - 0xffffffbffbdff000 ( 8 KB)

modules : 0xffffffbffc000000 - 0xffffffc000000000 ( 64 MB)

memory : 0xffffffc000000000 - 0xffffffc07fe00000 ( 2046 MB)

.init : 0xffffffc000902000 - 0xffffffc000949000 ( 284 KB)

.text : 0xffffffc000080000 - 0xffffffc0009015e4 ( 8710 KB)

.data : 0xffffffc000956000 - 0xffffffc0009c9000 ( 460 KB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4

NR_IRQS:64 nr_irqs:64 0

Architected cp15 timer(s) running at 25.00MHz (phys).

sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 2748779069440ns

Console: colour dummy device 80x25

Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=250000)

pid_max: default: 32768 minimum: 301

Security Framework initialized

Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)

Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)

Initializing cgroup subsys memory

Initializing cgroup subsys hugetlb

hw perfevents: enabled with arm/armv8-pmuv3 PMU driver, 7 counters available

EFI services will not be available.

CPU1: Booted secondary processor

Detected VIPT I-cache on CPU1

CPU2: Booted secondary processor

Detected VIPT I-cache on CPU2

CPU3: Booted secondary processor

Detected VIPT I-cache on CPU3

Brought up 4 CPUs

SMP: Total of 4 processors activated.

devtmpfs: initialized

DMI not present or invalid.

NET: Registered protocol family 16

Bman ver:0a02,02,01

qman-fqd addr 0xff800000 size 0x400000

qman-pfdr addr 0xfc000000 size 0x2000000

Qman ver:0a01,03,02

vdso: 2 pages (1 code @ ffffffc00095d000, 1 data @ ffffffc00095c000)

hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.

software IO TLB (4MB) mapped at

DMA: preallocated 256 KiB pool for atomic allocations

Serial: AMBA PL011 UART driver

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>

PTP clock support registered

bman-fbpr addr 0xfe000000 size 0x1000000

Bman err interrupt handler present

Bman portal initialised, cpu 0

Bman portal initialised, cpu 1

Bman portal initialised, cpu 2

Bman portal initialised, cpu 3

Bman portals initialised

Qman err interrupt handler present

QMan: Allocated lookup table at ffffff80001cd000, entry count 65537

QMan Pool Channel base 0x401

Parse QMan portal irq 41

Parse QMan portal irq 42

Parse QMan portal irq 43

Parse QMan portal irq 44

Parse QMan portal irq 45

Parse QMan portal irq 46

Parse QMan portal irq 47

Parse QMan portal irq 48

Parse QMan portal irq 49

Qman portal initialised, cpu 0

Qman portal initialised, cpu 1

Qman portal initialised, cpu 2

Qman portal initialised, cpu 3

Qman portals initialised

Bman: BPID allocator includes range 32:32

Qman: FQID allocator includes range 256:256

Qman: FQID allocator includes range 32768:32768

Qman: CGRID allocator includes range 0:256

Qman: pool channel allocator includes range 1025:15

No USDPAA memory, no 'usdpaa_mem' bootarg

fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller

fsl-ifc 1530000.ifc: IFC version 1.4, 8 banks

Switched to clocksource arch_sys_counter

NET: Registered protocol family 2

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 6, 262144 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP: reno registered

UDP hash table entries: 1024 (order: 3, 32768 bytes)

UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 29988K (ffffffc02043c000 - ffffffc022185000)

kvm : HYP mode not available

futex hash table entries: 1024 (order: 4, 65536 bytes)

audit: initializing netlink subsys (disabled)

audit: type=2000 audit(0.240:1): initialized

HugeTLB registered 2 MB page size, pre-allocated 0 pages

fuse init (API version 7.23)

9p: Installing v9fs 9p2000 file system support

io scheduler noop registered

io scheduler cfq registered (default)

layerscape-pcie 3500000.pcie: phy link never came up

layerscape-pcie 3500000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource

pci_bus 0000:00: root bus resource (bus address )

pci_bus 0000:00: root bus resource

pci 0000:00:00.0: BAR 1: assigned

pci 0000:00:00.0: BAR 0: assigned

pci 0000:00:00.0: BAR 6: assigned

pci 0000:00:00.0: PCI bridge to

layerscape-pcie 3600000.pcie: phy link never came up

layerscape-pcie 3600000.pcie: PCI host bridge to bus 0001:00

pci_bus 0001:00: root bus resource (bus address )

pci_bus 0001:00: root bus resource (bus address )

pci_bus 0001:00: root bus resource

pci 0001:00:00.0: BAR 1: assigned

pci 0001:00:00.0: BAR 0: assigned

pci 0001:00:00.0: BAR 6: assigned

pci 0001:00:00.0: PCI bridge to

PM: Power Management driver initialized.

Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled

console disabled

21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 26, base_baud = 25000000) is a 16550A

console enabled

21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 26, base_baud = 25000000) is a 16550A

21d0500.serial: ttyS2 at MMIO 0x21d0500 (irq = 27, base_baud = 25000000) is a 16550A

21d0600.serial: ttyS3 at MMIO 0x21d0600 (irq = 27, base_baud = 25000000) is a 16550A

brd: module loaded

loop: module loaded

ahci 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode

ahci 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst

scsi host0: ahci_platform

ata1: SATA max UDMA/133 mmio port 0x100 irq 34

60000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e

Amd/Fujitsu Extended Query Table at 0x0040

Amd/Fujitsu Extended Query version 1.3.

number of CFI chips: 1

10 ofpart partitions found on MTD device 60000000.nor

Creating 10 MTD partitions on "60000000.nor":

0x000000000000-0x000000100000 : "NOR bank0 RCW Image"

0x000000100000-0x000000200000 : "NOR bank0 U-Boot Image"

0x000000200000-0x000000300000 : "NOR bank0 U-Boot Env"

0x000000300000-0x000000400000 : "NOR bank0 FMan ucode"

0x000001100000-0x000003900000 : "NOR bank0 FIT Image"

0x000004000000-0x000004100000 : "NOR bank4 RCW Image"

0x000004100000-0x000004200000 : "NOR bank4 U-Boot Image"

0x000004200000-0x000004300000 : "NOR bank4 U-Boot Env"

0x000004300000-0x000004400000 : "NOR bank4 FMan ucode"

0x000005100000-0x000007900000 : "NOR bank4 FIT Image"

nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac

nand: Micron MT29F4G08ABBDAH4

nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64

Bad block table found at page 262080, version 0x01

Bad block table found at page 262016, version 0x01

3 ofpart partitions found on MTD device 7e800000.flash

Creating 3 MTD partitions on "7e800000.flash":

0x000000000000-0x000000100000 : "NAND U-Boot Image"

0x000000140000-0x000000142000 : "NAND U-Boot Env"

mtd: partition "NAND U-Boot Env" doesn't end on an erase block -- force read-only

0x000000200000-0x000001600000 : "NAND FIT Image"

fsl,ifc-nand 7e800000.nand: IFC NAND device at 0x7e800000, bank 1

m25p80 spi0.0: n25q128a13 (16384 Kbytes)

4 ofpart partitions found on MTD device spi0.0

Creating 4 MTD partitions on "spi0.0":

0x000000000000-0x000000100000 : "u-boot"

0x000000100000-0x000000600000 : "kernel"

0x000000600000-0x000000700000 : "dtb"

0x000000700000-0x000001000000 : "file system"

libphy: Fixed MDIO Bus: probed

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <[email protected]>

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

DBG: UUUUUUUUUUUUUU hcCh ?8?

<<>><<< p_LnxWrpFmDev->fmPhysBaseAddr = 0x1a00000

<<>><<< p_LnxWrpFmDev->fmBaseAddr = 0xffffff8008680000

Freescale FM module FMD API version 21.1.0

Freescale FM Ports module.

fsl_mac: fsl_mac: FSL FMan MAC API based driver

fsl_mac 1ae0000.ethernet: FMan MEMAC

fsl_mac 1ae0000.ethernet: FMan MAC address: 00:04:9f:03:dd:11

fsl_mac 1ae2000.ethernet: FMan MEMAC

fsl_mac 1ae2000.ethernet: FMan MAC address: 00:04:9f:03:dd:12

fsl_mac 1ae4000.ethernet: FMan MEMAC

fsl_mac 1ae4000.ethernet: FMan MAC address: 00:04:9f:03:dd:13

fsl_mac 1ae6000.ethernet: FMan MEMAC

fsl_mac 1ae6000.ethernet: FMan MAC address: 00:04:9f:03:dd:14

fsl_mac 1ae8000.ethernet: FMan MEMAC

fsl_mac 1ae8000.ethernet: FMan MAC address: 00:04:9f:03:dd:15

fsl_mac 1aea000.ethernet: FMan MEMAC

fsl_mac 1aea000.ethernet: FMan MAC address: 00:04:9f:03:dd:16

fsl_mac 1af0000.ethernet: FMan MEMAC

fsl_mac 1af0000.ethernet: FMan MAC address: 00:04:9f:03:dd:17

fsl_dpa: FSL DPAA Ethernet driver

fsl_dpa: fsl_dpa: Probed interface eth0

fsl_dpa: fsl_dpa: Probed interface eth1

ata1: SATA link down (SStatus 0 SControl 300)

fsl_dpa: fsl_dpa: Probed interface eth2

fsl_dpa: fsl_dpa: Probed interface eth3

fsl_dpa: fsl_dpa: Probed interface eth4

fsl_dpa: fsl_dpa: Probed interface eth5

fsl_dpa: fsl_dpa: Probed interface eth6

fsl_advanced: FSL DPAA Advanced drivers:

fsl_proxy: FSL DPAA Proxy initialization driver

fsl_dpa_shared: FSL DPAA Shared Ethernet driver

fsl_dpa_macless: FSL DPAA MACless Ethernet driver

fsl_oh: FSL FMan Offline Parsing port driver

e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI

e1000: Copyright (c) 1999-2006 Intel Corporation.

e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k

e1000e: Copyright(c) 1999 - 2014 Intel Corporation.

xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1

xhci-hcd xhci-hcd.0.auto: irq 31, io mem 0x02f00000

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

xhci-hcd xhci-hcd.1.auto: xHCI Host Controller

xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3

xhci-hcd xhci-hcd.1.auto: irq 32, io mem 0x03000000

hub 3-0:1.0: USB hub found

hub 3-0:1.0: 1 port detected

xhci-hcd xhci-hcd.1.auto: xHCI Host Controller

xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4

hub 4-0:1.0: USB hub found

hub 4-0:1.0: 1 port detected

xhci-hcd xhci-hcd.2.auto: xHCI Host Controller

xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 5

xhci-hcd xhci-hcd.2.auto: irq 33, io mem 0x03100000

hub 5-0:1.0: USB hub found

hub 5-0:1.0: 1 port detected

xhci-hcd xhci-hcd.2.auto: xHCI Host Controller

xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 6

hub 6-0:1.0: USB hub found

hub 6-0:1.0: 1 port detected

usbcore: registered new interface driver usb-storage

mousedev: PS/2 mouse device common for all mice

rtc-ds1307 0-0068: rtc core: registered pt7c4338 as rtc0

rtc-ds1307 0-0068: 56 bytes nvram

i2c /dev entries driver

imx2-wdt 2ad0000.wdog: timeout 60 sec (nowayout=0)

Driver 'mmcblk' needs updating - please use bus_type methods

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

sdhci-esdhc 1560000.esdhc: No vmmc regulator found

sdhci-esdhc 1560000.esdhc: No vqmmc regulator found

mmc0: SDHCI controller on 1560000.esdhc using ADMA 64-bit

platform caam_qi.0: Linux CAAM Queue I/F driver initialised

caam 1700000.crypto: Entropy delay = 3200

caam 1700000.crypto: Instantiated RNG4 SH0

caam 1700000.crypto: Instantiated RNG4 SH1

caam 1700000.crypto: device ID = 0x0a12060000000000 (Era 8)

caam 1700000.crypto: job rings = 4, qi = 1

caam algorithms registered in /proc/crypto

platform caam_qi.0: fsl,sec-v4.4 algorithms registered in /proc/crypto

caam_jr 1710000.jr: registering rng-caam

caam 1700000.crypto: fsl,sec-v4.4 algorithms registered in /proc/crypto

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

Freescale USDPAA process driver

fsl-usdpaa: no region found

Freescale USDPAA process IRQ driver

ipip: IPv4 over IPv4 tunneling driver

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 17

NET: Registered protocol family 15

bridge: automatic filtering via arp/ip/ip6tables has been deprecated. Update your scripts to load br_netfilter if you need this.

9pnet: Installing 9P2000 support

registered taskstats version 1

mmc0: new high speed SDHC card at address 0007

fsl_generic: FSL DPAA Generic Ethernet driver

fsl_generic: FSL DPAA Ethernet debugfs entries

rtc-ds1307 0-0068: setting system clock to 2016-02-25 14:43:55 UTC (1456411435)

fdt: not creating '/sys/firmware/fdt': CRC check failed

Waiting 5 sec before mounting root device...

mmcblk0: mmc0:0007 SD16G 14.6 GiB

mmcblk0: p1

usb usb5-port1: over-current condition

usb usb6-port1: over-current condition

RAMDISK: gzip image found at block 0

VFS: Mounted root (ext2 filesystem) on device 1:0.

EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended

VFS: Mounted root (ext2 filesystem) on device 179:1.

Trying to move old root to /initrd ... /initrd does not exist. Ignored.

Unmounting old root

Trying to free ramdisk memory ... failed

devtmpfs: error mounting -2

Freeing unused kernel memory: 284K (ffffffc000902000 - ffffffc000949000)

Freeing alternatives memory: 36K (ffffffc000949000 - ffffffc000952000)

Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.19.3+ #2

Hardware name: LS1043A RDB Board (DT)

Call trace:

[] secondary_start_kernel+0x124/0x134

---[ end Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

0 件の賞賛
返信