DDR3 throughput on p1010 RDB-PB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR3 throughput on p1010 RDB-PB

927 次查看
dmitri_kr
Contributor II

Hi,

On p1010-RDB-PB we see effective throughput of 185MB/s when doing DDR3 writes. Core frequency is 800MHz, DDR3 does not make any difference, we are getting same throughput at 266, 333 and 400 MHz DDR3 clock rates. When core frequency is increased to 1 GHz data rate goes up to 232MB/s.

Is this the expected throughput?

Thank you,

Dmitri

标记 (1)
0 项奖励
回复
2 回复数

801 次查看
alexander_yakov
NXP Employee
NXP Employee

Do you have data cache enabled for this memory region? Write-through or write-back?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

801 次查看
dmitri_kr
Contributor II

Hi Alexander,

Yes, I have copy-back cache enabled. A bit more info I am using vxworks bsp, DDR controller configuration is identical to the one from u-boot shipped with the development system.

Best regards,

Dmitri Krivchitch

0 项奖励
回复