DDR3 throughput on p1010 RDB-PB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 throughput on p1010 RDB-PB

716件の閲覧回数
dmitri_kr
Contributor II

Hi,

On p1010-RDB-PB we see effective throughput of 185MB/s when doing DDR3 writes. Core frequency is 800MHz, DDR3 does not make any difference, we are getting same throughput at 266, 333 and 400 MHz DDR3 clock rates. When core frequency is increased to 1 GHz data rate goes up to 232MB/s.

Is this the expected throughput?

Thank you,

Dmitri

タグ(1)
0 件の賞賛
2 返答(返信)

590件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Do you have data cache enabled for this memory region? Write-through or write-back?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

590件の閲覧回数
dmitri_kr
Contributor II

Hi Alexander,

Yes, I have copy-back cache enabled. A bit more info I am using vxworks bsp, DDR controller configuration is identical to the one from u-boot shipped with the development system.

Best regards,

Dmitri Krivchitch

0 件の賞賛