DDR Validation - endianness error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Validation - endianness error

Jump to solution
13,814 Views
sp_qoriq
Contributor III

I'm trying to use the DDR validation suite in QCVS to get optimal values for WRLVL registers for our custom board. We have the u-boot loading, but it fails to detect the DIMM capacity of channel 1 of 1st and 2nd memory controllers. I'm able to connect to the target and import the settings from the target as well. But the validation fails with "error: endianness". I have tried starting with Auto configuration and Import from Target configuration. udimm part is Mircon, MTA9ASF1G72AZ.

Sometimes I can get past the endianness error; but validation fails before the final step with some "internal error".

Reading from SPD also fails in the DDRv tool. Please see attached pictures. I have also attached the u-boot log for reference.

Can someone help me with these errors, please?

Thanks. 

0 Kudos
Reply
1 Solution
13,453 Views
addiyi
NXP Employee
NXP Employee

The issue is related with resetting the board over jtag. It could be because of incorrect RCW or because of some issue on jtag implementation. DDRv will reset the SoC before starting Read SPD action and will failed if it cannot do that.

A simple way to check this is to directly use ccs with the following commands:

delete all

config cc cwtap:<ip_addr>

ccs::config_chain {ls2085a dap}

display ccs::get_config_chain

ccs::reset_to_debug

If the message returned by the last command is Core not responding you should double check the jtag on your board.

Adrian

View solution in original post

0 Kudos
Reply
9 Replies
13,453 Views
sp_qoriq
Contributor III

We figured out the issue with our JTAG circuit. Thanks for the help addiyi‌

0 Kudos
Reply
13,453 Views
sdhunna
Contributor I

We are seeing similar errors for our custom board bring-up.  Can I ask what you changed in your JTAG that got this working for you?

0 Kudos
Reply
9,415 Views
pb3
Contributor II
I know that's it's kinda old topic - but have you managed to solve it? Was it a JTAG issue? If so, how did you manage to solve it?
0 Kudos
Reply
13,453 Views
sp_qoriq
Contributor III

Thanks for the reply, addiyi‌. That is exactly the error I'm seeing along with - "Subcore error encountered during multicore operation". Please see below:

(bin) 19 % ccs::reset_to_debug
Received CMD_RESET_TO_DEBUG
Sending CMD_SERVER_ALIVE
Sending CMD_SERVER_ALIVE
Sending CMD_SERVER_ALIVE
nhti command done - Subcore error encountered during multicore operation
Received CMD_PARSE_ERROR
nhti command done - Ok
LS2085A: Core not responding

Also, I can see that the SoC is going through the reset when DDRv starts reading from SPD. Is CCS unhappy because reset is not complete within certain seconds? Based on what I see on the CPU/CCS console, "Subcore error ...." message is printed out around the same time as the "Programming Controller %d" step of DDR initialization...   

But, our jtag seems to be working fine. We have used it extensively (breakpoints/examine memory, etc.) to debug the u-boot bringup. Anything in particular we should pay attention to?

0 Kudos
Reply
13,454 Views
addiyi
NXP Employee
NXP Employee

The issue is related with resetting the board over jtag. It could be because of incorrect RCW or because of some issue on jtag implementation. DDRv will reset the SoC before starting Read SPD action and will failed if it cannot do that.

A simple way to check this is to directly use ccs with the following commands:

delete all

config cc cwtap:<ip_addr>

ccs::config_chain {ls2085a dap}

display ccs::get_config_chain

ccs::reset_to_debug

If the message returned by the last command is Core not responding you should double check the jtag on your board.

Adrian

0 Kudos
Reply
13,453 Views
sp_qoriq
Contributor III

As you can see from the pictures/logs, the SoC used is LS2088A, rev 1.1. Appreciate the help...

0 Kudos
Reply
13,453 Views
sp_qoriq
Contributor III

QCVS version is: 4.10.0.0001-20170917. Running on Windows-10.

0 Kudos
Reply
13,453 Views
addiyi
NXP Employee
NXP Employee

Also provide the SoC used.

Adrian

0 Kudos
Reply
13,453 Views
addiyi
NXP Employee
NXP Employee

What is your QCVS version and your running OS?

Adrian

0 Kudos
Reply