Codewarrior TAP Suddenly Failing to Connect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior TAP Suddenly Failing to Connect

1,324件の閲覧回数
wbanning
Contributor I

I'm using Codewarrior 10.0.8 for the ARMv7 to program a custom board based on the LS1021A-TWR.  It had been working for the most part, I was able to program the PBL, u-boot and write additional files into NOR Flash.  However, it recently began consistently failing to start a debug session.  It always returns the error "CCSProtocolPlugin : Failed to correctly configure the JTAG chain".  Additionally, my RCW/u-boot binaries no longer seem to run from Flash the way they used to.  Does anyone know how I could debug this?

0 件の賞賛
返信
1 返信

1,265件の閲覧回数
ufedor
NXP Employee
NXP Employee

Provided description corresponds to absent/erased RCW in the NOR Flash.

To recover the board please take a look at the CW_ARMv7_Targeting_Manual (\ARMv7\Help\PDF\), Chapter 8 JTAG Configuration Files, to see how RCW override can be used for board recovery. Useful for your situation are chapter 8.2 and 8.3.

Also Chapter 4 Board recovery from https://community.nxp.com/servlet/JiveServlet/downloadBody/332382-102-2-269233/AN5184_Programing_SD_..., provides the necessary steps for board recovery.

0 件の賞賛
返信