Cannot boot T4250 QDS board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot boot T4250 QDS board.

Jump to solution
6,165 Views
colindavidson
Contributor II

Hello everyone, I have just started working on a T4240 QDS board. At first it wasn't giving me either a Yocto linux or UBoot command line, so I set the DIP switches to the "default" position in the quick-start guide, forgetting to save the original settings. Now I have the board failing in the U-boot sequence immediately after detecting the DDR3 ram ("Waiting for D_INIT timeout. Memory may not work."). Any suggestions for which settings to change?

0 Kudos
Reply
1 Solution
5,710 Views
ufedor
NXP Employee
NXP Employee

Please try to change in the default settings only SW1 to 0x17 - to get RCW from NOR Flash.

View solution in original post

0 Kudos
Reply
9 Replies
5,710 Views
ufedor
NXP Employee
NXP Employee

Hello,

Please provide the U-Boot booting log.

What are all on-board inscriptions and markings?

Do you have set the configuration switches as follows?

SW1= 0x24     SW2= 0xfe    SW3= 0x00 SW4= 0x50    SW9= 0x1f

    SW5= 0xe2     SW6= 0x0f    SW7= 0xfa     SW8= 0xcd    

0 Kudos
Reply
5,710 Views
colindavidson
Contributor II

Currently my settings are:

sw1: 0x24  sw2: 0xFF   sw3: 0x18  sw4: 0x50  sw5: 0xE2  sw6: 0x0F  sw7: 0xFA  sw8: 0xCF  sw9: 0x1F

With these settings, I get this at boot on the serial console:

U-Boot 2013.10-00403-g281afa2 (Nov 28 2013 - 13:18:35)

CPU0:  T4240E, Version: 2.0, (0x82480020)

Core:  e6500, Version: 2.0, (0x80400120)

Clock Configuration:

       CPU0:2083.333 MHz, CPU1:2083.333 MHz, CPU2:2083.333 MHz, CPU3:2083.333 MHz,

       CPU4:2083.333 MHz, CPU5:2083.333 MHz, CPU6:2083.333 MHz, CPU7:2083.333 MHz,

       CPU8:2083.333 MHz, CPU9:2083.333 MHz, CPU10:2083.333 MHz, CPU11:2083.333 MHz,

       CCB:833.333 MHz,

       DDR:852.516 MHz (1705.033 MT/s data rate) (Asynchronous), IFC:208.333 MHz

       FMAN1: 555.556 MHz

       FMAN2: 416.667 MHz

       QMAN:  416.667 MHz

       PME:   416.667 MHz

L1:    D-cache 32 KiB enabled

       I-cache 32 KiB enabled

Reset Configuration Word (RCW):

       00000000: 14180019 0c101914 00000000 00000000

       00000010: 04383063 30548c00 1c020000 1d000000

       00000020: 00000000 ee0000ee 00000000 000307fc

       00000030: 00000000 00000000 00000000 00000020

Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x26, vBank: 0

FPGA: v3 (T4240QDS_2012_1113_1114), build 438 on Tue Nov 13 17:14:23 2012

SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz

I2C:   ready

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM 9JSF25672AZ-2G1KZ

Detected UDIMM 9JSF25672AZ-2G1KZ

Detected UDIMM 9JSF25672AZ-2G1KZ

Waiting for D_INIT timeout. Memory may not work.

Waiting for D_INIT timeout. Memory may not work.

Waiting for D_INIT timeout. Memory may not work.

4 GiB left unmapped

With the default settings from the quick start guide (the ones you give), I get no serial output at boot.

0 Kudos
Reply
5,710 Views
colindavidson
Contributor II

Correction, I was looking at the DCM, which of course, being disabled, gave no output...

Booting with the default settings (SW1= 0x24     SW2= 0xfe    SW3= 0x00 SW4= 0x50    SW9= 0x1f     SW5= 0xe2     SW6= 0x0f    SW7= 0xfa     SW8= 0xcd)

gave the following serial console output:

U-Boot 2013.10-00403-g281afa2 (Nov 28 2013 - 13:18:35)

CPU0:  T4240E, Version: 2.0, (0x82480020)

Core:  e6500, Version: 2.0, (0x80400120)

Clock Configuration:

       CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,

       CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,

       CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,

       CCB:666.667 MHz,

       DDR:1600 MHz (3200 MT/s data rate) (Asynchronous), IFC:166.667 MHz

       FMAN1: 444.444 MHz

       FMAN2: 333.333 MHz

       QMAN:  333.333 MHz

       PME:   333.333 MHz

L1:    D-cache 32 KiB enabled

       I-cache 32 KiB enabled

Reset Configuration Word (RCW):

       00000000: 14180019 0c101914 00000000 00000000

       00000010: 04383063 30548c00 1c020000 1d000000

       00000020: 00000000 ee0000ee 00000000 000307fc

       00000030: 00000000 00000000 00000000 00000020

Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x26, vBank: 0

FPGA: v3 (T4240QDS_2012_1113_1114), build 438 on Tue Nov 13 17:14:23 2012

SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz

I2C:   ready

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM 9JSF25672AZ-2G1KZ

DDR clock (MCLK cycle 625 ps) is faster than the slowest DIMM(s) (tCKmin 938 ps) can support.

The choosen cas latency 37 is too large

Detected UDIMM 9JSF25672AZ-2G1KZ

DDR clock (MCLK cycle 625 ps) is faster than the slowest DIMM(s) (tCKmin 938 ps) can support.

The choosen cas latency 37 is too large

Detected UDIMM 9JSF25672AZ-2G1KZ

DDR clock (MCLK cycle 625 ps) is faster than the slowest DIMM(s) (tCKmin 938 ps) can support.

The choosen cas latency 37 is too large

Error: board specific timing not found for data rate 3199 MT/s

Trying to use the highest speed (2140) parameters

Error: board specific timing not found for data rate 3199 MT/s

Trying to use the highest speed (2140) parameters

Error: board specific timing not found for data rate 3199 MT/s

Trying to use the highest speed (2140) parameters

Error: WRREC doesn't support more than 16 clocks

Warning: CWL is out of range

Error: unsupported write recovery for mode register wr_mclk = 24

Error: unsupported cas latency for mode register

Warning: CWL is out of range

Error: WRREC doesn't support more than 16 clocks

Warning: CWL is out of range

Error: unsupported write recovery for mode register wr_mclk = 24

Error: unsupported cas latency for mode register

Warning: CWL is out of range

Error: WRREC doesn't support more than 16 clocks

Warning: CWL is out of range

Error: unsupported write recovery for mode register wr_mclk = 24

Error: unsupported cas latency for mode register

Warning: CWL is out of range

Waiting for D_INIT timeout. Memory may not work.

Waiting for D_INIT timeout. Memory may not work.

Waiting for D_INIT timeout. Memory may not work.

4

0 Kudos
Reply
5,711 Views
ufedor
NXP Employee
NXP Employee

Please try to change in the default settings only SW1 to 0x17 - to get RCW from NOR Flash.

0 Kudos
Reply
5,710 Views
colindavidson
Contributor II

Thanks, that did the trick.

0 Kudos
Reply
5,710 Views
addiyi
NXP Employee
NXP Employee

Please try using rcw + uboot for latest Freescale SDK, which is SDK 1.8.

Adrian

0 Kudos
Reply
5,710 Views
colindavidson
Contributor II

Hi Adrian,

I don't see how I can try your suggestion (assuming I understand it). Won't I need to boot to a prompt to be able to load this RCW and uboot? My problem is I can't boot the board in the first place. I'm probably not understanding you - can you tell me how to do this or point me at a manual that explains it?

Thanks,

Colin

0 Kudos
Reply
5,710 Views
addiyi
NXP Employee
NXP Employee

You could use CodeWarrior to flash images to NOR, even the board is not booting. But, seems Fedor ask your question and your board is up and running.

Adrian

0 Kudos
Reply
5,710 Views
colindavidson
Contributor II

I will check when I get home, where the system is. Unfortunately I'm on the road Today.

0 Kudos
Reply