Can B4860 boot from eMMC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can B4860 boot from eMMC?

1,314 Views
samyu
Contributor I

Can B4860 boot from eMMC instead of NOR Flash? I am not sure, if official answer is yes, I can make a decision to move on. Otherwise it takes too much risk.

Thanks all.

0 Kudos
Reply
1 Reply

1,230 Views
ufedor
NXP Employee
NXP Employee

Booting from eSDHC controller is supported.

The eSDHC controller is compatible with the MMC system specification version 4.2.

Considering aforesaid and that eMMC Specification confirms backwards compatibility with legacy MMC cards, booting from eMMC should be possible.

0 Kudos
Reply