Can B4860 boot from eMMC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can B4860 boot from eMMC?

1,322件の閲覧回数
samyu
Contributor I

Can B4860 boot from eMMC instead of NOR Flash? I am not sure, if official answer is yes, I can make a decision to move on. Otherwise it takes too much risk.

Thanks all.

0 件の賞賛
返信
1 返信

1,238件の閲覧回数
ufedor
NXP Employee
NXP Employee

Booting from eSDHC controller is supported.

The eSDHC controller is compatible with the MMC system specification version 4.2.

Considering aforesaid and that eMMC Specification confirms backwards compatibility with legacy MMC cards, booting from eMMC should be possible.

0 件の賞賛
返信