CPU LS1043A USB interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPU LS1043A USB interface

2,043 Views
julien_cavallo
Contributor IV

Dear Sir,

I have a question about the USB controller of the LS1043A CPU.

There is a limit (a time out value) in time versus the activation of the USB_DRVVBUS output and the return of the USB PHY VBUS input or not ?

A time limit between the activation of the USB power and the return of the 5V USB vias a USB curent limit component.

Thank in advance for your reply.

Best regards.

0 Kudos
Reply
2 Replies

2,012 Views
ufedor
NXP Employee
NXP Employee

There is no such timeout implemented in software.

0 Kudos
Reply

2,012 Views
julien_cavallo
Contributor IV

Hi ufedor,

Thank you for your fast reply.

Best regards

0 Kudos
Reply