CPU LS1043A RGMII interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU LS1043A RGMII interface

2,050件の閲覧回数
julien_cavallo
Contributor IV

Dear Sir,

I developp a custom board with the LS1043A CPU.

I have some questions about the RGMII interface of the CPU.

In my custom board, the RGMII interface of the CPU (EC1) is connected to a stacked connector to use it with a daughter board for debug only.

In most time, the daughter board is not connected, so the RGMII signals are left open.

I think, it is good to add pull-down resistors on all RGMII RX pins on the CPU board to avoid noise input when the debug daughter board is not connected.

So, could you confirm me  if it is necessary to add pull-down resistors on all RX RGMII signals (EC1_RXD0 to EC1_RXD3, EC1_RX_DV, EC1_RX_CLK and EC1_GTX_CLK125) to avoid RX RGMII bus open.

Thank you in advance for your reply.

Best regards 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,008件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, it is a good idea to add pull down resistors to input RGMII signals. 10K is enough value for resistors.

Regards,

Bulat

0 件の賞賛
返信

2,008件の閲覧回数
julien_cavallo
Contributor IV

Hi Bulat,

Thank you for your quick respond.

Best regards.

0 件の賞賛
返信