CPU LS1043A RGMII interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CPU LS1043A RGMII interface

2,100 次查看
julien_cavallo
Contributor IV

Dear Sir,

I developp a custom board with the LS1043A CPU.

I have some questions about the RGMII interface of the CPU.

In my custom board, the RGMII interface of the CPU (EC1) is connected to a stacked connector to use it with a daughter board for debug only.

In most time, the daughter board is not connected, so the RGMII signals are left open.

I think, it is good to add pull-down resistors on all RGMII RX pins on the CPU board to avoid noise input when the debug daughter board is not connected.

So, could you confirm me  if it is necessary to add pull-down resistors on all RX RGMII signals (EC1_RXD0 to EC1_RXD3, EC1_RX_DV, EC1_RX_CLK and EC1_GTX_CLK125) to avoid RX RGMII bus open.

Thank you in advance for your reply.

Best regards 

标记 (1)
0 项奖励
回复
2 回复数

2,058 次查看
Bulat
NXP Employee
NXP Employee

Yes, it is a good idea to add pull down resistors to input RGMII signals. 10K is enough value for resistors.

Regards,

Bulat

0 项奖励
回复

2,058 次查看
julien_cavallo
Contributor IV

Hi Bulat,

Thank you for your quick respond.

Best regards.

0 项奖励
回复