CCSProtocolPlugin : error writing memory CCS last error : Scan timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CCSProtocolPlugin : error writing memory CCS last error : Scan timeout

1,961 次查看
mgkiller
Contributor III

Hi all,

 

After finishing execute P4040DS_init_core_cacheon.tcl(this *.tcl goes well),  when i run my demoP4040-core0_RAM_P4040_Cache_Download in CodeWarrior 10.1,it pups out an error and stop,(you can see the print message within the Console Window in console.log as attachment)

"CCSProtocolPlugin : error writing memory,CCS last error : Scan timeout".

Does it meat the USBTAP can't download my *.elf into P4040 internal Cache?

And why not?anyone help me?

 

Here is my development environment

CPU:P4040 DDR2:512MB ( a custom board )

CW:"CodeWarrior Development Studio for PA" " v1.0.0.FSL_b03045"

CW Project & tcl: same as P4040DS



Any help is appreciated!


Original Attachment has been moved to: P4040DS_init_core_cacheon.txt.zip

Original Attachment has been moved to: console.txt.zip

标记 (2)
0 项奖励
回复
0 回复数