CCS error logs during the DDR validation test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCS error logs during the DDR validation test

1,170 Views
akhilesh_nema
Contributor IV

Why does the following log appear during DDR validation tests?

CCSAPI connection #1 accepted from ABC-localhost at Fri Feb 21 07:40:55 2025
check_min_version(serverh=0,*version)
  api version: 00000004 00000006
ccs_get_cc_config(*config_string, count)
  ERROR(23): CC not present
setup_cc(serverh=0,config_string= cwtap )
*** unhandled(command=169) ***

 

Do I have a setup related issue?

(Desktop) 17 % show version
CCS Windows Release Build 503.0.0.220812-p0
CodeWarrior Connection Server version {4.13}
(C) Copyright 2003-2015 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED
(C) Copyright 2016-2021 NXP 
(Desktop) 18 % 
Tags (1)
0 Kudos
Reply
1 Reply

1,143 Views
LFGP
NXP TechSupport
NXP TechSupport
dear akhilesh_nema,
the messages log is related to the CW TAP connection problems, please be sure your CW TAP is recognized, follow the steps mentioned in the "CodeWarrior TAP Probe User Guide" manual, also, please be sure your CW license is active.

https://www.nxp.com/docs/en/user-guide/CWTAPUG.pdf
0 Kudos
Reply