Build error SDK v1.8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build error SDK v1.8

2,035件の閲覧回数
sandratrujillog
Contributor III

Hello,

I'm trying to build the version full with the SDK v1.8 but I get the following error:

DEBUG: Executing shell function do_install
install: cannot stat 'fsl_fman_ucode_t2:t2080*.bin': No such file or directory
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_install (log file is located at /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.7362)

I am using the linux version 14.04.3. Could someone help me with this error? I have been able to compile the minimal version.

0 件の賞賛
返信
3 返答(返信)

1,713件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use the following command: bitbake fsl-image-full


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,713件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use Ubuntu 14. Do not use Ubuntu 16.

Usually the following command sequence is used for SDK installing under Ubuntu 14.04 64-bit:

  1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

 

  1. a) command: ls -l /bin/sh

                Message:  /bin/sh -> dash

  1. b) command: sudo dpkg-reconfigure dash

                Answer after password – No

                Message:

                Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

                Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

                Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

                Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

  1. c) command for checking: ls -l /bin/sh

                Message: /bin/sh -> bash

 

  1. mount SDK source .iso file
  2. cd <sdk-install-dir>.
  3. ./sources/meta-freescale/scripts/host-prepare.sh

Usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. bitbake fsl-image-minimal
  2. bitbake fsl-image-full


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,713件の閲覧回数
sandratrujillog
Contributor III

When I follow your instructions I find the following error:

user@user-VirtualBox:~/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release$ bitbake ces-image-full
WARNING: Unable to get checksum for ces-avio-m1553-native SRC_URI entry ces-avio-m1553-native-3.13.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-avio-m1553 SRC_URI entry ces-avio-m1553-3.13.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-avio-m1553 SRC_URI entry ces-avio-m1553-3.13.0.tar.gz: file could not be found
WARNING: Unable to get checksum for cesxpclib-native SRC_URI entry cesxpclib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesxpclib SRC_URI entry cesxpclib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesxpclib SRC_URI entry cesxpclib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesmaintenance-native SRC_URI entry cesmaintenance-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesmaintenance SRC_URI entry cesmaintenance-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesmaintenance SRC_URI entry cesmaintenance-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesnvramlib SRC_URI entry cesnvramlib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesnvramlib SRC_URI entry cesnvramlib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesflash-native SRC_URI entry cesflash-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesflash SRC_URI entry cesflash-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesflash SRC_URI entry cesflash-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-ipc-native SRC_URI entry ces-ipc-1.0.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-ipc SRC_URI entry ces-ipc-1.0.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-ipc SRC_URI entry ces-ipc-1.0.0.tar.gz: file could not be found

Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "powerpc-fsl-linux"
MACHINE = "mfcc-8558"
DISTRO = "fsl-networking"
DISTRO_VERSION = "QorIQ-SDK-V1.8"
TUNE_FEATURES = "m32 fpu-hard e6500 altivec"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "daisy:18837ea4cdd4fdab608e0a032a11a2dfb6b1ee1a"
meta-fsl-ppc = "daisy:ed8d8f097eb9fb9c4d76cfeb617da5ce72d9b414"
meta-fsl-toolchain = "daisy:a253b3594d8d9e0a4ed869d1fb502c395c4438ac"
meta-fsl-networking = "daisy:6eb28ed659bbadfa470237dfce98bcbf53c18fe1"
meta-virtualization = "daisy:df44ec7a68c8e4b713a458a5b93e903103dea85c"
meta-oe
meta-networking
meta-webserver
meta-ruby
meta-filesystems = "daisy:4a44c4107899363b22c01eb5621b0c86db1c659c"
meta-java = "daisy:65c89b93fa9d4c89e1dfb5b795075cbadb541009"
meta-openstack
meta-openstack-compute-deploy
meta-openstack-controller-deploy
meta-openstack-qemu = "daisy:c040904422eb3c13f7abb66996bed8d675ada860"
meta-ces
meta-mfcc-8558 = "<unknown>:<unknown>"

NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_install (log file is located at /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.31355)
ERROR: Logfile of failure stored in: /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.31355
Log data follows:
| DEBUG: Executing shell function do_install
| install: cannot stat 'fsl_fman_ucode_t2:t2080*.bin': No such file or directory
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.31355)
ERROR: Task 715 (/home/user/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-ppc/recipes-dpaa/fm-ucode/fm-ucode_git.bb, do_install) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3391 tasks of which 3096 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
  /home/user/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-ppc/recipes-dpaa/fm-ucode/fm-ucode_git.bb, do_install

0 件の賞賛
返信