Build error SDK v1.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build error SDK v1.8

2,031 Views
sandratrujillog
Contributor III

Hello,

I'm trying to build the version full with the SDK v1.8 but I get the following error:

DEBUG: Executing shell function do_install
install: cannot stat 'fsl_fman_ucode_t2:t2080*.bin': No such file or directory
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_install (log file is located at /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.7362)

I am using the linux version 14.04.3. Could someone help me with this error? I have been able to compile the minimal version.

0 Kudos
Reply
3 Replies

1,709 Views
Pavel
NXP Employee
NXP Employee

Use the following command: bitbake fsl-image-full


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,709 Views
Pavel
NXP Employee
NXP Employee

Use Ubuntu 14. Do not use Ubuntu 16.

Usually the following command sequence is used for SDK installing under Ubuntu 14.04 64-bit:

  1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

 

  1. a) command: ls -l /bin/sh

                Message:  /bin/sh -> dash

  1. b) command: sudo dpkg-reconfigure dash

                Answer after password – No

                Message:

                Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

                Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

                Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

                Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

  1. c) command for checking: ls -l /bin/sh

                Message: /bin/sh -> bash

 

  1. mount SDK source .iso file
  2. cd <sdk-install-dir>.
  3. ./sources/meta-freescale/scripts/host-prepare.sh

Usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. bitbake fsl-image-minimal
  2. bitbake fsl-image-full


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,709 Views
sandratrujillog
Contributor III

When I follow your instructions I find the following error:

user@user-VirtualBox:~/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release$ bitbake ces-image-full
WARNING: Unable to get checksum for ces-avio-m1553-native SRC_URI entry ces-avio-m1553-native-3.13.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-avio-m1553 SRC_URI entry ces-avio-m1553-3.13.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-avio-m1553 SRC_URI entry ces-avio-m1553-3.13.0.tar.gz: file could not be found
WARNING: Unable to get checksum for cesxpclib-native SRC_URI entry cesxpclib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesxpclib SRC_URI entry cesxpclib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesxpclib SRC_URI entry cesxpclib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesmaintenance-native SRC_URI entry cesmaintenance-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesmaintenance SRC_URI entry cesmaintenance-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesmaintenance SRC_URI entry cesmaintenance-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesnvramlib SRC_URI entry cesnvramlib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesnvramlib SRC_URI entry cesnvramlib-1.3.469.tar.gz: file could not be found
WARNING: Unable to get checksum for cesflash-native SRC_URI entry cesflash-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesflash SRC_URI entry cesflash-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for cesflash SRC_URI entry cesflash-1.0.32.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-ipc-native SRC_URI entry ces-ipc-1.0.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-ipc SRC_URI entry ces-ipc-1.0.0.tar.gz: file could not be found
WARNING: Unable to get checksum for ces-ipc SRC_URI entry ces-ipc-1.0.0.tar.gz: file could not be found

Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "powerpc-fsl-linux"
MACHINE = "mfcc-8558"
DISTRO = "fsl-networking"
DISTRO_VERSION = "QorIQ-SDK-V1.8"
TUNE_FEATURES = "m32 fpu-hard e6500 altivec"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "daisy:18837ea4cdd4fdab608e0a032a11a2dfb6b1ee1a"
meta-fsl-ppc = "daisy:ed8d8f097eb9fb9c4d76cfeb617da5ce72d9b414"
meta-fsl-toolchain = "daisy:a253b3594d8d9e0a4ed869d1fb502c395c4438ac"
meta-fsl-networking = "daisy:6eb28ed659bbadfa470237dfce98bcbf53c18fe1"
meta-virtualization = "daisy:df44ec7a68c8e4b713a458a5b93e903103dea85c"
meta-oe
meta-networking
meta-webserver
meta-ruby
meta-filesystems = "daisy:4a44c4107899363b22c01eb5621b0c86db1c659c"
meta-java = "daisy:65c89b93fa9d4c89e1dfb5b795075cbadb541009"
meta-openstack
meta-openstack-compute-deploy
meta-openstack-controller-deploy
meta-openstack-qemu = "daisy:c040904422eb3c13f7abb66996bed8d675ada860"
meta-ces
meta-mfcc-8558 = "<unknown>:<unknown>"

NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_install (log file is located at /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.31355)
ERROR: Logfile of failure stored in: /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.31355
Log data follows:
| DEBUG: Executing shell function do_install
| install: cannot stat 'fsl_fman_ucode_t2:t2080*.bin': No such file or directory
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /home/user/QorIQ-SDK-V1.8-20150619-yocto/build_mfcc-8558_release/tmp/work/ppce6500-fsl-linux/fm-ucode/git-r1/temp/log.do_install.31355)
ERROR: Task 715 (/home/user/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-ppc/recipes-dpaa/fm-ucode/fm-ucode_git.bb, do_install) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3391 tasks of which 3096 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
  /home/user/QorIQ-SDK-V1.8-20150619-yocto/meta-fsl-ppc/recipes-dpaa/fm-ucode/fm-ucode_git.bb, do_install

0 Kudos
Reply