Bug in QUICC Engine UART device driver for Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in QUICC Engine UART device driver for Linux

1,228 Views
HWLab
Contributor I

I have done some modifications on the Linux QUICC Engine UART device driver (ucc_uart.c) to control the DRT bit in UPSMR. During this work I found some code that has to be wrong. The problem is in qe_uart_set_termios() where all but the byte size part of UPSMR is cleared while I think the purpose was to clear only the byte size part. The result is that setting byte size isn't working correct. Most peaple are using 8 bit byte size and this is working, so I guess this is why this bug hasn't been found before. Switching from 8 bit to any other will fail.

Below is my suggestion on how to fix it.

--- clean_linux/linux/drivers/tty/serial/ucc_uart.c

+++ linux/drivers/tty/serial/ucc_uart.c

@@ -880,8 +885,8 @@

      */

     /* byte size */

-    upsmr &= UCC_UART_UPSMR_CL_MASK;

-    supsmr &= UCC_UART_SUPSMR_CL_MASK;

+    upsmr &= ~(UCC_UART_UPSMR_CL_MASK);

+    supsmr &= ~(UCC_UART_SUPSMR_CL_MASK);

     switch (termios->c_cflag & CSIZE) {

     case CS5:

@@ -911,6 +916,9 @@

         upsmr |= UCC_UART_UPSMR_SL;

         supsmr |= UCC_UART_SUPSMR_SL;

         char_length++;  /* + SL */

+    } else {

+        upsmr &= ~(UCC_UART_UPSMR_SL);

+        supsmr &= ~(UCC_UART_SUPSMR_SL);

     }

     if (termios->c_cflag & PARENB) {

@@ -928,6 +936,9 @@

             supsmr |= UCC_UART_SUPSMR_RPM_EVEN |

                 UCC_UART_SUPSMR_TPM_EVEN;

         }

+    } else {

+        upsmr &= ~(UCC_UART_UPSMR_PEN);

+        supsmr &= ~(UCC_UART_SUPSMR_PEN);

     }

     /*

0 Kudos
Reply
0 Replies