Hello,
Is there anyway to be able to re-run the program multiple times (on the DSP) without using 'tgreset' command?
On the first trial, 'dsp boot' dumps the following output:
Het Mgr 248 0
IPC: dsp_shared_size - 0x1000000
IPC: dsp_private_addr - 0x80000000
IPC: dsp_private_size - 0x7ff00000
IPC: shared_ctrl_addr - 0xfff00000
IPC: shared_ctrl_size - 0x100000
IPC: max_num_ipc_channels 64
IPC: max_channel_depth 16
fsl_shm module installed successfully withmajor num : 247
fsl_l1d Major=246 Minor=0
===B4860QDS DSP boot Application (3.0.0) ===
SYSTEM MAP
DSP PrivArea: Addr=80000000 Size=7ff00000
Shared CtrlArea: Addr=fff00000 Size=100000
DSP Core0 M2: Addr=0 Size=0
DSP Core1 M2: Addr=0 Size=0
DSP M3: Addr=c40000000 Size=8000
PA CCSRBAR: Addr =ffe000000 Size=1000000
DSP CCSRBAR: Addr =ffe000000 Size=1000000
DBG: Addr =0 Size=0
PA Shared Area: Addr=60000000 Size=f000000
DSP Shared Area: Addr=6f000000 Size=1000000
PA Debug Print Shared Area: Addr=0 Size=0
DSP Debug Print Shared Area: Addr=c40000000 Size=8000
Loading Dsp image eNBL1.bin
Copy Part 80000000 2c1bc
(repeated copying commands)
Copy Part a40b4000 32c42
intvec_addr =a405e000 in L1 Binary
Before StarCore release ========
LCC_BSTRH=0x0
LCC_BSTRL=0x7ffff000
LCC_BSTAR=0x8110000b
GCR_CDCER0=0x0
GCR_CHMER0=0x0
DCFG_BRR=0xf
After StarCore release ========
LCC_BSTRH=0x0
LCC_BSTRL=0xa405e000
LCC_BSTAR=0x8100000c
GCR_CDCER0=0x3f0
GCR_CHMER0=0x3f00
DCFG_BRR=0x3ff
BSTRL,BSTAR,CDCERO,CHMERO n DCFG_BRR set now
sleep 1, waiting for hw sem
sleep 1, waiting for hw sem
HS_MPR[1]=0xfe
HS_MPR[1]=0x0
== DSP Booted up ==
The next time I run 'dsp boot' without 'tgreset', I get the following output:
Het Mgr 248 0
IPC: dsp_shared_size - 0x1000000
IPC: dsp_private_addr - 0x80000000
IPC: dsp_private_size - 0x7ff00000
IPC: shared_ctrl_addr - 0xfff00000
IPC: shared_ctrl_size - 0x100000
IPC: max_num_ipc_channels 64
IPC: max_channel_depth 16
fsl_shm module installed successfully withmajor num : 247
fsl_l1d Major=246 Minor=0
===B4860QDS DSP boot Application (3.0.0) ===
SYSTEM MAP
DSP PrivArea: Addr=80000000 Size=7ff00000
Shared CtrlArea: Addr=fff00000 Size=100000
DSP Core0 M2: Addr=0 Size=0
DSP Core1 M2: Addr=0 Size=0
DSP M3: Addr=c40000000 Size=8000
PA CCSRBAR: Addr =ffe000000 Size=1000000
DSP CCSRBAR: Addr =ffe000000 Size=1000000
DBG: Addr =0 Size=0
PA Shared Area: Addr=60000000 Size=f000000
DSP Shared Area: Addr=6f000000 Size=1000000
PA Debug Print Shared Area: Addr=0 Size=0
DSP Debug Print Shared Area: Addr=c40000000 Size=8000
Loading Dsp image eNBL1.bin
Copy Part 80000000 2c1bc
(repeated copying commands)
Copy Part a40b4000 32c42
intvec_addr =a405e000 in L1 Binary
Before StarCore release ========
LCC_BSTRH=0x0
LCC_BSTRL=0xa405e000
LCC_BSTAR=0x8100000c
GCR_CDCER0=0x3f0
GCR_CHMER0=0x3f00
DCFG_BRR=0x3ff
After StarCore release ========
LCC_BSTRH=0x0
LCC_BSTRL=0xa405e000
LCC_BSTAR=0x8100000c
GCR_CDCER0=0x3f0
GCR_CHMER0=0x3f00
DCFG_BRR=0x3ff
BSTRL,BSTAR,CDCERO,CHMERO n DCFG_BRR set now
sleep 1, waiting for hw sem
sleep 1, waiting for hw sem
Infinitely repeated (sleep 1, waiting for hw sem)
Am I missing something?
Is there a way to reset the DSP without using 'tgreset'?
Thanks,