Boot from SPI NOR flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot from SPI NOR flash?

ソリューションへジャンプ
2,148件の閲覧回数
trondwang
Contributor I

Hi NXP,

the reference board LS1043ARDB-PA/PB has a SPI NOR flash (U32). Is it possible to boot from a SPI NOR flash by a RCW setting?

regards

Trond Inge

タグ(1)
0 件の賞賛
返信
1 解決策
2,012件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, booting from this device is supported. Please refer to deployment guide in Linux SDK documentation precise instruction.

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-3E22804D-DD1E-43D7-AF28-8...


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,013件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, booting from this device is supported. Please refer to deployment guide in Linux SDK documentation precise instruction.

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-3E22804D-DD1E-43D7-AF28-8...


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信