Boot P2041RDB-PB from SD Card?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot P2041RDB-PB from SD Card?

ソリューションへジャンプ
2,896件の閲覧回数
cquick
Contributor I

Hello,

I have been reading the documentation for the P2041RDB-PB, but I cannot seem to figure out how to get u-boot to boot from an SD card.

I followed the instructions here: Booting to Linux from an SD Card/MMC for P2040/P2041 but that is just for Linux, not for u-boot. I have been looking and looking and just cannot find anywhere how I can accomplish this.

Does anyone have some sort of guide on how to load u-boot from an SD card, and also all of the Linux stuff, so that everything is completely booting from SD.

Thank you!

タグ(5)
0 件の賞賛
返信
1 解決策
2,145件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look P2041 Reference Manual, Table 4-30, bits 196-200 "BOOT_LOC" field for boot location options.

There is no SD card listed as boot option, so direct booting from SD card is not supported.

To boot via PBI please look the following link:

Freescale Technical Information Center

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,146件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look P2041 Reference Manual, Table 4-30, bits 196-200 "BOOT_LOC" field for boot location options.

There is no SD card listed as boot option, so direct booting from SD card is not supported.

To boot via PBI please look the following link:

Freescale Technical Information Center

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信