BCM5461

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BCM5461

1,497 Views
jinghui_mou1
Contributor I

In our case, BCM5461s is used as RGMII PHY, but this IP ping does not work . We can use MDIO access PHY and see auto-negotiation  done. Should we have to build firmware and do NXP has patch for it ?

0 Kudos
Reply
1 Reply

1,370 Views
bpe
NXP Employee
NXP Employee

Some PHYs do require downloadable microcode, it also may be necessary
to patch the OS or bootloader you are working with. Consult at the PHY
manufacturer for required software/updates. For QorIQ processors

equipped with DPAA,  a RAM-based FMAN microcode is required. You don't
have to build it, ready binaries for processors are available:

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply