BCM5461

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BCM5461

1,498件の閲覧回数
jinghui_mou1
Contributor I

In our case, BCM5461s is used as RGMII PHY, but this IP ping does not work . We can use MDIO access PHY and see auto-negotiation  done. Should we have to build firmware and do NXP has patch for it ?

0 件の賞賛
返信
1 返信

1,371件の閲覧回数
bpe
NXP Employee
NXP Employee

Some PHYs do require downloadable microcode, it also may be necessary
to patch the OS or bootloader you are working with. Consult at the PHY
manufacturer for required software/updates. For QorIQ processors

equipped with DPAA,  a RAM-based FMAN microcode is required. You don't
have to build it, ready binaries for processors are available:

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信