B4860 SerDes Lane Naming Check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

B4860 SerDes Lane Naming Check

ソリューションへジャンプ
1,932件の閲覧回数
samjackson
Contributor II

Hi - quick question;

B4860 QoriQ Reference Manual Section 26 name lanes A, B, C, D, E, F, G, H.

Pinout in B4860 Data Sheet shows the lanes a 0, 1, 2 etc.

Can I confirm: Lane A = 0, Lane B = 1 etc etc?

Is there a reason why they are named differently between the documents?

Many thanks,

Sam

0 件の賞賛
返信
1 解決策
1,849件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, lane names A, B, C, D, E, F, G, H correspond to the lanes signals numbers 0, 1, 2, 3, 4, 5, 6, 7. Please see Table 26-4. SerDes1 Mapping in the B4860 QoriQ Reference Manual. I.e. in the manual the serdes signals are numbered too - see Table 3-1. B4860 Signal Reference by Functional Block.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,850件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, lane names A, B, C, D, E, F, G, H correspond to the lanes signals numbers 0, 1, 2, 3, 4, 5, 6, 7. Please see Table 26-4. SerDes1 Mapping in the B4860 QoriQ Reference Manual. I.e. in the manual the serdes signals are numbered too - see Table 3-1. B4860 Signal Reference by Functional Block.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,849件の閲覧回数
samjackson
Contributor II

Thanks Serguei.

0 件の賞賛
返信