Action erase flash on T1040 board loop forever ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Action erase flash on T1040 board loop forever ?

791 次查看
tienphamxuan
Contributor I

Hello, I meet a problem with T1040 flash programing. When i erase flash on T1040 board the erasing task running forever :

fl::target -lc "T1040-core00_SRAM_T1040_Download"
fl::target -b 0x0 0x40000
fl::target -v off -l off
cmdwin::fl::device -d "S29GL256P" -o "16Mx16x1" -a 0xe8000000 0xe9ffffff
cmdwin::fl::protect all off
 Beginning Operation ...    
-------------------------
Performing target initialization ...    
 Downloading Flash Diagnostics Driver ...   
 Reading flash ID ...
Unprotecting all sectors...   
Unprotecting ...   
Unprotecting ....   
Unprotecting .....   
Unprotecting ......   
 Unprotect Command Succeeded    
cmdwin::fl::device -sd all
cmdwin::fl::device -se 0
cmdwin::fl::erase list
-------------------------
 Downloading Flash Device Driver ...   
 Reading flash ID ...
Erasing Sector 0xE8000000 to 0xE801FFFF   
 Erasing .............................................................
 
Erasing ..   
 Erasing .............................................................
 
Erasing ..   
 Erasing .............................................................
 
Erasing ..   
 Erasing ......................

Anyone can help me ?

0 项奖励
回复
1 回复

680 次查看
tienphamxuan
Contributor I

Hi all, thanks for reviewed. I solved this problem by myself. I disable BTCL signal on NOR IFC bus.

0 项奖励
回复