About UART operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About UART operation

3,226 次查看
kojimiura
Contributor III
UART2_SIN is pulled down with 10kΩ.
When not using UART2 (DUART registers remain at their initial values)
1. Will it harm my device?
2. Would you like to receive data?
3. Is it possible for the CPU to be interrupted for some reason?
4. Is it okay if the Divisor setting value is zero?
Thank you.
0 项奖励
回复
6 回复数

3,142 次查看
yipingwang
NXP TechSupport
NXP TechSupport

When not using UART2 , the response for the above-stated queries are as follows:
1. Will it harm my device
No

2. Would you like to receive data?
No

3. Is it possible for the CPU to be interrupted for some reason?
No

4. Is it okay if the Divisor setting value is zero?
Does not matter.

0 项奖励
回复

3,187 次查看
kojimiura
Contributor III

What do you think after that?

0 项奖励
回复

3,182 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 项奖励
回复

3,086 次查看
kojimiura
Contributor III

Since the internal clock of UART2 is disabled, Start bit is not detected. Is this understanding correct?

0 项奖励
回复

3,079 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

0 项奖励
回复

3,076 次查看
kojimiura
Contributor III
Thank you.
0 项奖励
回复