Hi,
I am using T2080 in my application in this I planned to connect S70GL02GS12FHIV20 nor flash to the IFC bus. I planned to use x16 bit external latch for address/date demux application. How to interface this devices, My flash is having 27bit addressing.
Regards,
Rajesh
Connections should be as shown in RM Figures 13-277, 13-326
ADM MODE 0, CSOR0[ADM_SHFT]=4
[IFC_AD[0:15],IFC_AVD] -> latch -> A[26:11]
IFC_A[20:30] -> A[10:0]
IFC_AD[0:15] <-> DQ[15:0]
IFC_CS0# -> CE#
IFC_OE# -> OE#
IFC_WE0# -> WE#
IFC_WP0# -> WP#
IFC_RB0# -> R/B#
1.8V -> VIO
3.3V -> VCC
PORESET# -> RESET#
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for the recommendation, As per your recommendation I need to provide latch for 16bits(AD0 to AD15) instead I have connected like this whether this will work ?
IFC_A[16:30] -> A[14:0]
[IFC_AD[4:15] -> latch -> A[26:15]
IFC_AD[0:15] <-> DQ[15:0]
IFC_CS0# -> CE#
IFC_OE# -> OE#
IFC_WE0# -> WE#
IFC_WP0# -> WP#
IFC_RB0# -> R/B#
1.8V -> VIO
3.3V -> VCC
Regards,
Rajesh
Yes. It will work.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------